2023-11-13 12:54 AM
Hi all,
I am trying to configure burst dma on my board (stm32g474). I have successfully configure the dma for single register, however, when I want to configure dma for more than one register, I failed to do that as it only allow me to fill one address for DMA Src address when 2 channels should be updated. Do anyone know how should I configure the DMA Src address if I want to use dma to update 2 respective dma channel?
2023-11-13 2:45 AM
Hello @OFN
If I understand correctly the question, you need to increment source and destination address by the number of data items (already in CNDTR before being decremented) to the second DMA channel. Then, you can configure the parameters and enable the second DMA channel.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-22 8:07 AM - edited 2023-12-01 4:49 AM
Let me share with you some additional information!
Here the Figure 258. from RM0440 on HRTIM chapter (especially 27.3.23).
On the overview below, there are 3 types of registers :
It is only necessary to have the DMA controller pointing to the HRTIM_BDMADR register as
the destination, in the memory, to the peripheral configuration with the peripheral increment
mode disabled.
Once you write in HRTIM_BDMADR, it's automatically triggers (no need Burst DMA source):
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.