cancel
Showing results for 
Search instead for 
Did you mean: 

Getting HAL_ERROR while using I2C in Fast mode pulse

Advance_tech
Associate III

Hi All,

I trying to interface MAX6651 Device using I2C module using STM32F410C8U6 MCU.

Device address is 0x36 But when i'm using 

HAL_FMPI2C_IsDeviceReady(&hfmpi2c1, 0x36 , 2, 100); this API returning the value
HAL_ERROR.

Here are some snaps

Screenshot 2023-11-07 151633.pngScreenshot 2023-11-07 151523.png

Anybody look into it send some solutions

 

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Pierre_Paris
ST Employee

Hello @Advance_tech,

Thank you for your question.

In the MAX6650 document from Analog Devices you shared, it specified that the rise/fall time should be between 20ns and 300ns (cf the figure below) 

PierrePARIS_0-1699449191054.png

But on your CubeMx screenshot, you enter 0 ns, please change it and try again.

Let me know !

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

I think I2C start bit not generating.

FMPI2C1->CR1 |= (1 << 0);

FMPI2C1->CR2 |= (1 << 13);

printf("Hi\r\n");

while(!(FMPI2C1->CR2 & (1 << 13)));

printf("Hello\r\n");

 

program is struct inside the while(1)

after while(1) nothing is executing.

Is there is any chance the I2C Peripheral is gone


please answer

 

hi @Pierre_Paris 

uint32_t error_code = HAL_FMPI2C_GetError(&hfmpi2c1);

 

i am getting error code as 2 that means

HAL_FMPI2C_ERROR_ARLO arbitration error

please let me know what are the causes of this error

Pierre_Paris
ST Employee

Hello @Advance_tech,

Several I2C multi-masters can be connected to the same I2C bus and operate concurrently. By constantly monitoring SDA and SCL for start and stop conditions, they can determine whether the bus is currently idle or not. If the bus is busy, masters delay pending I2C transfers until a stop condition indicates that the bus is free again.

However, it may happen that two masters start a transfer at the same time. During the transfer, the masters constantly monitor SDA and SCL. If one of them detects that SDA is low when it should actually be high, it assumes that another master is active and immediately stops its transfer. This process is called arbitration.

Here some remark :

  • Have you corrected the rise/fall time ?
  • How many masters does your I2C bus have ? 
  • Check your data frame with an analyzer if possible
  • Do you switch the I2C device on your microcontroller between slave and master mode in your code ?

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hi @Pierre_Paris 

we have single master and two slave devices in I2C line.

HAL_FMPI2C_IsDeviceReady(&hfmpi2c1, max6551_add_2 , 1, 2000);

when i use this API error code is 32 means timeout error

 

HAL_FMPI2C_Master_Transmit(&hfmpi2c1, i,(uint8_t *)&pdata, sizeof(pdata), HAL_MAX_DELAY);

when i use this API the error code is 2 means arbitration error.

Pierre_Paris
ST Employee

Hello @Advance_tech,

Before I investigate further, can you please confirm you corrected the rise/fall time. (Timeout fault can be the consequence because the slave cannot follow...)

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hi @Pierre_Paris thanks for quick response

i have given rise time and fall time as 300ns as mentioned in datasheet.

But i don't know how to calculate rise time and fall time  

Pierre_Paris
ST Employee

Hello @Advance_tech,

300ns is the maximum limit value, please check with 200ns (just in case).

You don't need to calculate rise and fall time. There is, indeed, a calculation with the I2C_TIMINGR but it's unnecessary to do it (tools do). However, if you want to learn more, you can read the chapter 2.2.4 of AN4235 by clicking here.

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Pierre_Paris  i would like to thank for all your responses. i slowly heading into solve the problem.

retval = HAL_FMPI2C_IsDeviceReady(&hfmpi2c1, max6551_add_2, 1, 100);

error_code = HAL_FMPI2C_GetError(&hfmpi2c1);

 

printf("return value %d\r\n",retval);

HAL_Delay(100);

printf("error code is = %ld\r\n",error_code);

HAL_Delay(100);

Now i getting HAL_BUSY From this HAL_FMPI2C_IsDeviceReady API and error code is 32 which means

HAL_FMPI2C_ERROR_TIMEOUT

please let me know what may cause these problems