cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 HRTIM BURST DMA CONFIGURATION

OFN
Associate II

Hi all,

I am trying to configure burst dma on my board (stm32g474). I have successfully configure the dma for single register, however, when I want to configure dma for more than one register, I failed to do that as it only allow me to fill one address for DMA Src address when 2 channels should be updated. Do anyone know how should I configure the DMA Src address if I want to use dma to update 2 respective dma channel?

2 REPLIES 2
FBL
ST Employee

Hello @OFN 

If I understand correctly the question, you need to increment source and destination address by the number of data items (already in CNDTR before being decremented) to the second DMA channel. Then, you can configure the parameters and enable the second DMA channel. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!
Pierre_Paris
ST Employee

Hello @OFNand @FBL,

 

Let me share with you some additional information!

Here the Figure 258. from RM0440 on HRTIM chapter (especially 27.3.23).

On the overview below, there are 3 types of registers :

  • HRTIM_BDMADR (Burst DMA data register) : DMA unique destination (burst operation is started by the first write access in this register)
  • Registers to update for your application (eg : HRTIM_PERBR, HRTIM_CMP1BR....)
  • 6 update registers multiplexing HRTIM_BDMADR  to the register you want to update. (HRTIM handles internally the data re-routing to the final destination register).

Pierre_P_0-1701433519823.png

It is only necessary to have the DMA controller pointing to the HRTIM_BDMADR register as
the destination, in the memory, to the peripheral configuration with the peripheral increment
mode disabled.

Once you write in HRTIM_BDMADR, it's automatically triggers (no need Burst DMA source):

  • The copy of the data value into the registers enabled in BDTxUPR and BDMUPR register
    bits
  • The increment of the register pointer to the next location to be filled

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.