2025-01-07 08:06 AM - last edited on 2025-01-07 08:35 AM by Andrew Neil
Hello STM Community,
I'm facing an issue with my STM32 device on Windows 11. The Virtual COM Port (VCP) driver is not working, and in the Device Manager, the device is shown as:
Unknown USB Device (Device Descriptor Request Failed)
Here are the details:
Despite these efforts, the problem persists.
Has anyone else encountered this issue with Windows 11? Are there any additional steps or settings I need to configure to resolve this?
Thank you for your assistance!
Best regards,
A.Sujith
2025-01-07 08:12 AM
Is this a VCP you are implementing, or the one in an ST-Link?
Have you tried any other Windows version?
Or any other OS?
What hardware are you using?
What software/middleware?
What tools & versions?
2025-01-07 08:17 AM
Hello,
Are you sure you are using a good USB cable? try to change the cable.
2025-01-07 08:20 AM
This board works fine on other laptops and previously worked well on this laptop too. However, now the driver is not being detected. I uninstalled and reinstalled the driver, which temporarily fixed the issue, but the problem reappeared, and the driver is no longer working.
2025-01-07 08:34 AM - edited 2025-01-07 08:36 AM
@Sujith wrote:This board works fine on other laptops and previously worked well on this laptop too.
So what's changed on that laptop?
What's now different between that laptop and the others?
(Thread title edited to clarify this).