2024-07-03 02:01 AM
Hello,
I am looking for STM with the following features:
- 48 pin (could be 64 pin only if BGA)
- 4 I2C interfaces
- 1 ADC channel
- most important: lowest price possible
Could somebody suggest several P/N I could check?
Adam
2024-07-03 03:58 AM - edited 2024-07-03 04:02 AM
Hello @adams1 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to use our ST-MCU-FINDER-PC - STM32 and STM8 product finder for desktops - STMicroelectronics . It will help you to find the suitable MCU for your use case. It is also integrated in the STM32CubeMX If you don't wont to download a new app.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.