cancel
Showing results for 
Search instead for 
Did you mean: 

STM low price 4xI2C, 48 pin

adams1
Associate

Hello,

I am looking for STM with the following features:

- 48 pin (could be 64 pin only if BGA)

- 4 I2C interfaces

- 1 ADC channel

- most important: lowest price possible

Could somebody suggest several P/N I could check?

 

Adam

1 REPLY 1
STTwo-32
ST Employee

Hello @adams1 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to use our ST-MCU-FINDER-PC - STM32 and STM8 product finder for desktops - STMicroelectronics . It will help you to find the suitable MCU for your use case. It is also integrated in the STM32CubeMX If you don't wont to download a new app.

STTwo32_0-1720004531325.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.