2024-10-31 1:30 AM - edited 2024-10-31 1:39 AM
Hy,
I have tried to resample a 16bit/8kHz audio signal to 16kHz and 48kHz.
Conversion works, but the audio is noisy. I am tested it on development board STM32H747 CM7 core.
I have tried libraries: SRC236_CM7_GCC.a and SRC236HQ_CM7_GCC.a without quality improvement.
I am working with 10ms blocks.
Initialization parameters are:
// conversion from 8kHz to 16kHz
src236_static_param_t src236_static_param.src_mode = SRC236_RATIO_2;
// library initialization
src_error = src236_reset(PSrc236PersistentMem_ToCodecOut, PSrcScratchMem_ToCodecOut);
if (src_error != SRC236_ERROR_NONE)
{
return (-1); //error AUDIO_ERROR_SRC
}
/* SRC236 effect static parameters setting */
src_error = src236_setParam(&src236_static_param, PSrc236PersistentMem_ToCodecOut);
if (src_error != SRC236_ERROR_NONE)
{
return (-1); //error AUDIO_ERROR_SRC
}
// 8kHz, 16 bit audio input // 10ms block
LowRateConversionBuff_ToCodecOut.nb_channels = 1;
LowRateConversionBuff_ToCodecOut.nb_bytes_per_Sample = 2;
LowRateConversionBuff_ToCodecOut.mode = NOT_INTERLEAVED;
// LowRateConversionBuff_ToCodecOut.data_ptr = //set data pointer before usage
LowRateConversionBuff_ToCodecOut.buffer_size = 80;
// 16kHz, 16bit audio output
HighRateConversionBuff_ToCodecOut.nb_channels = 1;
HighRateConversionBuff_ToCodecOut.nb_bytes_per_Sample = 2;
HighRateConversionBuff_ToCodecOut.mode = NOT_INTERLEAVED;
// HighRateConversionBuff_ToCodecOut.data_ptr = //set data pointer before usage
HighRateConversionBuff_ToCodecOut.buffer_size = 160;
Processing part:
LowRateConversionBuff_ToCodecOut.data_ptr = pInData;
HighRateConversionBuff_ToCodecOut.data_ptr = pOutData;
src_error = src236_process(&LowRateConversionBuff_ToCodecOut, &HighRateConversionBuff_ToCodecOut, PSrc236PersistentMem_ToCodecOut);
if (src_error == SRC236_ERROR_NONE)
{
return 0;
}
Solved! Go to Solution.
2024-11-08 12:06 AM
Thank you for your helps, it was my fault.
I sometimes processed the same packet of data more times. It generated a noise when a new packet started.
After a repair, audio quality is good, both in normal, and in HQ modes, too.
Anyway I am extracted the resample functionality from X-CUBE-AUDIO-KIT, for IIR mode, 16 bit data, without any malloc, OS functionality, and it works too.
2024-10-31 1:34 AM
Please see the posting tips for how to properly post source code:
2024-10-31 1:20 PM
Dear @KBéla.1 ,
It may happen you are using a Library not compatible yet with STM32H7 series . let us know which version are you using .
You can check this link : X-CUBE-AUDIO-KIT - Audio processing software expansion for STM32Cube - STMicroelectronics
If you are using this Library : X-CUBE-AUDIO - Audio effects software expansion for STM32Cube - STMicroelectronics you can see
Hope it helps
STOne-32.
2024-11-04 12:53 AM
I tried SRC236 lib version: V1.0.3 , from
X-CUBE-AUDIO v1.1.1, and it is noisy. The only parameter which I can change is the audio block size, which can be a mono or stereo signal. Now I am using 10ms Mono audio blocks, which not works.
Now I am going to try resample functionality from X-CUBE-AUDIO-KIT. I can`t find documentation for it, but the sources are available, so I hope, I can do it.
Thanks for the info
2024-11-04 1:11 AM
@KBéla.1 wrote:X-CUBE-AUDIO-KIT. I can`t find documentation for it
Did you see:
https://www.st.com/en/embedded-software/x-cube-audio-kit.html#documentation
In particular, UM3297, Getting started with X-CUBE-AUDIO-KIT
2024-11-08 12:06 AM
Thank you for your helps, it was my fault.
I sometimes processed the same packet of data more times. It generated a noise when a new packet started.
After a repair, audio quality is good, both in normal, and in HQ modes, too.
Anyway I am extracted the resample functionality from X-CUBE-AUDIO-KIT, for IIR mode, 16 bit data, without any malloc, OS functionality, and it works too.
2024-11-08 1:20 AM
Great @KBéla.1 ! very happy to see you made it working.