2017-11-07 12:24 AM
Hello every body we are using stm32f103xx microcontrollers , we want to send our data by wireless using spirit1 module ,
- is it possible ?
-which library is suitable ?
-what about distance amd range of gigahertz modules ?
urgent help needed plz thanks
Samah Tarhan
Argebilisim
Solved! Go to Solution.
2017-11-16 03:27 AM
Ä° SOLVE it it was a wrong adapter from hyperterminal to ttl , before i used adm now i use usb dongle ch340g or arduino adapter . now i communicate perfectly with my spirit 1 ,thanks
2017-11-07 01:17 AM
Surely, the answer to this will be found by reading the documentation for this '
spirit1 module'?
You have done that, haven't you ... ?
(it's not by any means new - but it is certainly still applicable!)2017-11-07 02:22 AM
Ah - you mean this:
http://www.st.com/en/wireless-connectivity/spirit1.html
Loads of documents on that page for you to read!
Just looking at the very first paragraph of the Dev Kit User Manual:
The kit includes a SPIRIT1 development kit graphical user interface (SPIRIT1 DK - GUI) which allows checking the SPIRIT1 main performance and easily measure parameters such as sensitivity, output power and main features of the SPIRIT1. It alsocontains SPIRIT1 firmware libraries for STM32L
and STM8L to allow development of SPIRIT1 applications.2017-11-07 02:40 AM
thanks so much mister Andrew ,, so it will not be possible to use on my stm32f103xx series maybe from another libraries ? ,
-what about transmition range ??
also i got another question if we use the STM32ML and wmbus is it free standart or needs fees ?
2017-11-07 02:48 AM
yes i mean gıgahertz modules spml1 of st 868 or 915 , i need to establish my network collecting data and send them to pc
2017-11-07 04:27 AM
TARHAN SAMAH wrote:
so it will not be possible to use on my stm32f103xx series maybe from another libraries ? ,
Eh??
:(
What on earth makes you think that??
2017-11-07 05:18 AM
you mean the sp1ml is usable on stm32f103xx??? can you explain more , i dont understand
2017-11-07 06:12 AM
Did you read:
?2017-11-07 06:34 AM
Might need to be ported. Seem to remember there being a sub-ghz radio on L4 IoT board.
Range tends v to help highly dependent on power, antenna and line of sight.
LoRa which can be used as sub-ghz radio can get 11km LoS without much effort, but about 1km in more obstructed use.
2017-11-07 08:27 AM
Everything you post to the forum is 'urgent', please read the Hacker FAQ to understand how such requests are interpreted.
http://www.catb.org/esr/faqs/smart-questions.html#urgent