SPI HW NSS Incompatibility between STM32H7 and STM32F4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-29 4:40 AM
Hello ,
I am migrating code from STM32H7 to STM32F4
I face the following problems with SPI,
1-Hardware output NSS pulses is activated only with HAL_SPI_Init/HAL_SPI_DeInit.
2-There should be a pull up on the NSS in order to reach 3.3V and it can't work with default push-pull configuration.
3-Can't find a mode for pulsated NSS like that in STM32H7
What I meas by pulsated NSS is that the NSS is released after each SPI byte/halfword , automatically in burst transmission and DMA modes.
This way the SPI DMA is almost useless ,because I need to monitor the end of SPI transmission in order to release and reassert NSS manually.
How can I overcome this problem?
- Labels:
-
SPI
-
STM32F4 Series
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-29 6:57 AM
> How can I overcome this problem?
As you found out, the 'F4 does not have the NSS Pulsing feature, this appeared in the STM32 somewhat later than the 'F4.
As a workaround, at the cost of several pins and one or two timers, you can generate NSS framing using timers; the details depend on your application.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-29 7:13 AM
There are two problems in this proposal
1-how to sync timer with DMA
2-in DMA mode without pulsating NSS , the clock is contiues and there's no time between each send byte and the next to pulsate NSS
next picture shows the required behavior as it runs on STM32H743
next picture shows what happen without pulsating NSS
there's no time between bytes to intorduce NSS pulse manually using timer or GPIO
The only solution which I have now is using SW NSS and send SPI data byte by byte -No DMA and no Bursts- but the problems is that it's much s;lower and the overhead on controller as shown in next picture
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-29 11:10 AM
The simplest solution is to feed the SPI Tx from DMA triggered by a channel of the same timer which generates the framing. Care must be taken if there's significant load on the given DMA and related buses.
A more secure but also more complex solution, at the cost of two timers and some pins is, to generate both SCK and framing by the timers, and feed them back to SPI, which is run as a slave.
A mix of these two approaches might be possible, or other solutions too. You have to have a good command of the timers and SPI; this is not something simply clickable in CubeMX.
You may want to have a look and at the TI mode - it's not the same as pulsing between frames, but maybe it fits your slaves' requirements (of which you've told us nothing yet).
Or simply drop the 'F4 and have a look at some other more modern family.
JW