2019-03-15 5:25 AM
Hello ,
With SPI (SPI2 in my case) I experience a delay between a wite to TXDR and the start of the SCK activity in case of an empty TX fifo. It seems to be something like 5 SCK periods, so it changes with SCK frequency but this ratio remains. I checked with several values of MBR. The ratio is a little smaller for higher frequencies ie the delay is shorter in terms of SCK periods.
This effect is largest at the first transmission after enabling SPI and reduces to a ratio of about 3 for subsequent transmissions, but only if TX fifo is empty when TXDR is written.
Sending back to back and inserting some delay with MIDI works fine when I write several values to TXDR in a row.
(My findings after some experiments)
Any idea why that is and how to get rid of it?
Thanks a lot
Martin
2019-03-15 6:34 AM
Some more information:
frequent repeats of writing to TXDR results in delay times between 3.25 and 4.25 SCK cycles, measured at 417 kHz.