2015-09-07 2:34 AM
Hello,
I have some problems with FMC when I try to port my code from SMT32F407(with FSMC interface) to new project based on STM32F746(with FMC). The only changes I've made are timings(adapted to 216 MHz clock) and init structures(FSMC => FMC). I have also SRAM connected to the same data and address bus and it works well, so I think that my hardware is ok and problem is inside init code. Thus, I have few questions: is there any difference between using FMC on STM32F4 and STM32F7? Should I change or add something in initialisation code when using FMC on STM32F7? #nor-flash-fmc-stm32f72015-09-11 2:31 AM
You were right. It looks like FMC address region belongs to 'External RAM', thus it is cacheable by default.
I solved problem by adding MPU region that covers NOR memory address, here is the code: http://pastebin.com/BdG6j1vL With this D-Cache can be enabled and it doesn't impact NOR memory. I wonder why FMC_NOR example project from SMT32756G_EVAL works with enabled D-Cache and disabled MPU. Thanks for clarification.2015-09-15 2:40 AM
> I wonder why FMC_NOR example project from SMT32756G_EVAL works with enabled D-Cache and disabled MPU.
Can't this be because the example uses the memory only as a plain memory, whereas you attempted to read the ID, which means different data output by memory at the same address. Memory mapped peripherals would present a similar ''hardware volatility'' problem. JW2015-12-17 2:48 PM
Hello, is the cache enabled by default on FMC SRAM Bank 1 ? I am trying to port the FMC code used to interface with an ILI9325 LCD controller from STM32F4 to STM32F7. When doing a simple clear screen :
loop for 320x240 pixels :
*(data address 0x60020000) = color 0xFF00;it seems some instructions aren't sent to the controller or aren't registered by the controller. Thus, only a third of the screen is cleared. Surprinsingly, adding a 1ms delay between instructions solves it. Changing SRAM Timing didn't help. Hardware is identical between both F4/F7 boards. Thank you.
2015-12-17 11:56 PM
Yes, this is the same problem as the original poster had. Use the MPU.
JW2015-12-22 3:29 AM
I'd just like to thank everyone for their help on this subject.
I had the same issue with the NOR flash on the STM32F7 eval board (and am also wondering how the NOR examples work without setting the MPU)In the end, all I had to do was call this to setup the MPU for the 128Mbit NOR Flash memory on the F7 Eval board:static void MPU_Config(void){ MPU_Region_InitTypeDef MPU_InitStruct; /* Disable the MPU */ HAL_MPU_Disable(); /* Configure the MPU attributes for 16Mb NOR Flash*/ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x60000000; MPU_InitStruct.Size = MPU_REGION_SIZE_16MB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enable the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);}