2024-08-01 5:22 PM
Using a stm32f303RE Nucleo board which has 4 (independent ?) ADC blocks.
I'm trying to read a single channel from each of the 4 ADC under DMA simultaneously triggered from the same timer update event but I'm only getting about 30-40% of the data I'm asking for. Note that using 4 channels of a single ADC would result in skew as the reads would be sequential so I'd loose timing accuracy
A single channel works fine (ADC1/Chan 1) and using HAL_ADC_Start_DMA() with a length of 500, SamplingTime of ADC_SAMPLETIME_2CYCLES_5 triggered from TIM2 at 800KHz I get what I'd expect.
Running ADC2/Chan 5 at the same time (same speed & parameters) results in both blocks only receiving about 200 words of good data followed by 300 words of garbage (values close to 0). Adding ADC3 & ADC4 gets progressively less valid data.
What comes to mind are the following questions:
At present I have no other interrupt or DMA activity but eventually I'll be sampling Timer capture with another 4 DMA channels so if its a memory bandwidth issue I'm sunk!
Solved! Go to Solution.
2024-08-02 7:51 PM
Solved - silly typo had the memory array for the 4 DMA channels the 'wrong way round' !!
2024-08-02 7:13 PM
Further information:
Each of the 4 ADC blocks read the same values (+/- 5 counts) even though 2 out of the 4 have their inputs grounded.
They are supposed to be reading a 40KHz sinewave signal but it looks like I have nearly 100% crosstalk between ADCs.
2024-08-02 7:51 PM
Solved - silly typo had the memory array for the 4 DMA channels the 'wrong way round' !!