2018-07-04 09:38 AM
Hi,
I haven't been able to get the sensorTile Datalog SDcard application to run without having SWD connected from the Nucleo ST-link, or by issuing a reset by shorting SWD pins 3 and 5 on the sensorTile cradle board. I need this to boot up without issuing a reset. Had this issue in the past with another STM32L4 project but cannot remember the solution. Anyone know?
I'm using the sensorTile STEVAL-STLKT01V1 kit. I need the sensorTile and the smaller cradle board with battery to run standalone once power boots up.
Thanks,
Kevin