cancel
Showing results for 
Search instead for 
Did you mean: 

Selecting Micro for touch display application

Ricko
Senior III

Hi,

I have not developed graphic applications before and am trying to figure out how do I select an STM32 micro for a touch-display application using TouchGFX (if relevant to the question).

The display I am looking at has an SDI interface and this is the link to the product page: 3.4" DSI Round Touch Display (800x800) | The Pi Hut

And this to the Wiki: 3.4inch DSI LCD (C) - Waveshare Wiki

Thank you

 

1 ACCEPTED SOLUTION

Accepted Solutions
Zhou JianQiang
Senior II

Hi 

Note not all stm32 support DSI, so first you can use stm32cubemx to select which one support DSI.

then you can refer https://support.touchgfx.com/docs/category/hardware-components for details. 

View solution in original post

2 REPLIES 2
Zhou JianQiang
Senior II

Hi 

Note not all stm32 support DSI, so first you can use stm32cubemx to select which one support DSI.

then you can refer https://support.touchgfx.com/docs/category/hardware-components for details. 

Thank you @Zhou JianQiang