2014-07-04 4:58 AM
2014-07-04 11:31 AM
Does the similar code work on the STM32F429I-DISCO?
How does the pin/board configuration differ? I'd dig deeper but none of your pin configuration is commented, and there's no schematic.2014-07-05 5:23 AM
Thank you for your reply
I have tested today with the STM32F429i discovery and that seems to work correctly. Even when I stop the program in the debugger mode for a couple of minutes beforereading back the data. The data is still valid. I will show the differences between the pins on the discovery and our project:Discovery: (uses ISSI 64Mb sdram - http://www.issi.com/WW/pdf/42-45S16400J.pdf)// PB5 = SDCKE1 (CKE) PF0 = A0// PB6 = SDNE1 (/CS) PF1 = A1// PC0 = SDNWE (/WE) PF2 = A2// PD0 = D2 PF3 = A3// PD1 = D3 PF4 = A4// PD8 = D13 PF5 = A5// PD9 = D14 PF11 = SDNRAS (/RAS)// PD10 = D15 PF12 = A6// PD14 = D0 PF13 = A7// PD15 = D1 PF14 = A8// PE0 = NBL0 (LDQM) PF15 = A9// PE1 = NBL1 (UDQM) PG0 = A10// PE7 = D4 PG1 = A11// PE8 = D5 PG4 = BA0 (BANK A0)// PE9 = D6 PG5 = BA1 (BANK A1)// PE10 = D7 PG8 = SDCLK (CLK)// PE11 = D8 PG15 = SDNCAS (/CAS)// PE12 = D9// PE13 = D10// PE14 = D11// PE15 = D12Our project: (uses Alliance Memory 512 Mb sdram - http://www.alliancememory.com/pdf/dram/512M-SDRAM.pdf)// *PH7 = SDCKE1 (CKE) PF0 = A0// *PH6 = SDNE1 (/CS) PF1 = A1// PC0 = SDNWE (/WE) PF2 = A2// PD0 = D2 PF3 = A3// PD1 = D3 PF4 = A4// PD8 = D13 PF5 = A5// PD9 = D14 PF11 = SDNRAS (/RAS)// PD10 = D15 PF12 = A6// PD14 = D0 PF13 = A7// PD15 = D1 PF14 = A8// PE0 = NBL0 (LDQM) PF15 = A9// PE1 = NBL1 (UDQM) PG0 = A10// PE7 = D4 PG1 = A11// PE8 = D5 *PG2 = A12// PE9 = D6 PG4 = BA0 (BANK A0)// PE10 = D7 PG5 = BA1 (BANK A1)// PE11 = D8 PG8 = SDCLK (CLK)// PE12 = D9 PG15 = SDNCAS (/CAS)// PE13 = D10 *PH12 = VDD SDRAM enable// PE14 = D11// PE15 = D12* means different from STM32F429i discoveryI hope this will inform you a little bit better.My sincerly2014-07-05 6:17 AM
FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_8b;
FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b; Isn't the geometry of this part 13 Rows, 10 Columns?
2014-07-05 6:51 AM
Yeah, you are absolutely right. We have missed that one.
Changed it in the sofware but this doesn't effect the memory loss problem.2014-07-07 12:26 AM
The line
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD |
RCC_AHB1Periph_GPIOE | RCC_AHB1Periph_GPIOF | RCC_AHB1Periph_GPIOG | RCC_AHB1Periph_GPIOG, ENABLE);
references GPIOG twice. You don't appear to enable GPIOH clock.
2015-05-10 1:53 PM
Hey did you solve this problem ? i have simmilar one with AS4C4M16S-6TIN. but after delay i have following results:
2002ffd8 de111206d00003d4 fe117206so as you can see two octets are changed and i have no ideal what can make this, any sugestions ?2015-05-10 6:26 PM
Would seem to suggest you have some issue with D13/D14, or with the refresh period?
2015-05-11 11:46 AM
datasheet says ''Refresh Interval Time - max 15.6 '' so :
//15.6us*84MHz=1311 when i use 100 FMC_Bank5_6->SDRTR=100<<1;this didnt gave any result.when i puteven
FMC_Bank5_6->SDRTR=10000<<1;
thats didnt gave any result.
Would seem to suggest you have some issue with D13/D14
could you explain me this part, and how to check it ?2015-05-11 12:28 PM
could you explain me this part, and how to check it ?
You'd revisit your board as designed via the schematic. Verify that you're using the right pins.You'd evaluate your board as built, looking at a) the bare PCB board, and b) a finished one, and probe out the lines to verify continuity, and lack of shorts.At a software level you could write and immediate read several locations with different combinations of bit patterns in the D13 and D14 position, and confirm with zero delay if the bits ever hold zero states, or the correct states.These would seem like some pretty basic steps to validate the design. If those work, then focus on the software and timing, and review signals with a scope or logic analyzer, until you understand what's actually going on.