cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO Bit Start Error with STM32F407VGT6 and STM32CubeMX

silas
Associate II
Posted on January 11, 2015 at 20:46

I'm having problems with communication through SDIO. In the initialization process, where are only sent commands, everything works, but the function HAL_SD_SendSDStatus is returning SD_START_BIT_ERR.

Informations about the circuit and firmware:

-STM32CubeMX v4.5.0 and STM32F4 library v1.3.0

-Clock always 400kHz (to ensure that I will not have problems with the bus speed in the tests)

-It uses the internal pull-up of the microcontroller

-Several sd cards were tested, all of them >=4GB and >=class 4, with FAT32

After debugging, I found that the problem happens in the code snippet (below) of the file stm32f4xx_hal_sd.c within the HAL_SD_SendSDStatus function:

   

/* Configure the SD DPSM (Data Path State Machine) */

    sdio_datainitstructure.

DataTimeOut

=

SD_DATATIMEOUT

;

    sdio_datainitstructure.

DataLength

= 64;

    sdio_datainitstructure.

DataBlockSize

=

SDIO_DATABLOCK_SIZE_64B

;

    sdio_datainitstructure.

TransferDir

=

SDIO_TRANSFER_DIR_TO_SDIO

;

    sdio_datainitstructure.

TransferMode

=

SDIO_TRANSFER_MODE_BLOCK

;

    sdio_datainitstructure.

DPSM

=

SDIO_DPSM_ENABLE

;

    SDIO_DataConfig(hsd->

Instance

, &sdio_datainitstructure);

   

/* Send ACMD13 (SD_APP_STAUS)  with argument as card's RCA */

    sdio_cmdinitstructure.

Argument

= 0;

    sdio_cmdinitstructure.

CmdIndex

=

SD_CMD_SD_APP_STAUS

;

    SDIO_SendCommand(hsd->

Instance

, &sdio_cmdinitstructure);

Before call the SDIO_DataConfig function, the SDIO_STA register is 0, after call this function, the bits RXFIFOE and RXACT goes to 1, what is expected. After call the function SDIO_SendCommand with the command ACMD13, the bits RXFIFOE and RXACT goes to 0 and the bits STBITERR and CMDREND goes to 1. Here is where the problem happens.

Could anyone help me with this?

thanks,

Silas

#sdio #wait-for-you--clive1-!-!-! #stm32 #stm32f4 #sd
2 REPLIES 2
emailalternativo
Associate
Posted on January 12, 2015 at 21:37

Hi,

I'm developing a project that uses SD card and I am having the same problem described here. Silas, if you solve this problem or somebody here knows how to solve, please, let me know.

iisla.1
Associate

is the question relevant?