2023-01-17 5:57 PM
I have the following two wrapper functions:
void POT_Load_Value(uint16_t value)
{
uint8_t w[2];
w[0] = 0; //reg
w[1] = value;
I2C_Write(POT_ADDR, w, 2);
}
uint8_t I2C_Write(uint8_t device, uint8_t *pValues, uint8_t size)
{
if (HAL_OK == HAL_I2C_Master_Transmit_IT(&hi2c1, device, pValues, size))
return I2C_SUCCESS;
else
return I2C_ERR;
}I am using a simple callback:
void HAL_I2C_MasterTxCpltCallback(I2C_HandleTypeDef *hi2c)
{
if (hi2c == &hi2c1)
ISR.I2C_dacTxComplete;
}I am not sure how the I2C works on this device which brings me to the question:
The calling function POT_Load_Value variable w. Do I have to worry about scope being lost here between the transmission of the first byte and then the second? Should I be using static here?
2023-01-17 6:41 PM
Yes, scope collapses immediately.
Static if you serialize operation so it won't reenter.
Allocate dynamically for a more general approach.