Same code from STM32L476RG won't run on one core of STM32H747.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-12 4:20 PM
On a my Nucleo-L476RG board, I used cube to only activate an LED connected gpio (PA5) - Nothing else.
Then I programmed some blinky code into the main while loop:
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, RESET);
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, SET);
HAL_Delay(1000);
Then I `Generate Code', and start debugging.
The LED blinks as expected.
Then I move to my STM32H747I-Disco board with a STM32H747XIH.
File, New, STM32 Project ( MCU Selector Screen opens and I select `STM32H747XI', Next.
I name my project 747XIH_NoRtos. and open in MX perspective.
In System Core I click GPIO pin I15 ands et it to GPIO Output. I do not select RTOS.
I click Project, Generate Code.
A file structure with a branch for CM4 and a branch for CM7 is created.
Under CM4, Core, Src, main.c,
I enter similar blinky code in the main while loop.
Under CM4 I Generate Code and get 0 errors, 0 warnings.
Then Build All and again 0 error, 0 warnings.
I click on Run, Debug, leaving debug configuration at default.
The error(16) says to, `Please specify the serial number in the debug config’.
Serial number of what?
I assume I’m using ST Link built onto my DISCO board.
Are there other things I need to change in the debug configuration?
- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-12 9:03 PM
https://www.openstm32.org/forumthread1586
follow above link
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-12 9:58 PM
Not sure if that link applies, I'm running a single STM32H747I-Disco with the dual core M4/M7.
My code is operating out of the M4.
I have a single ST Link using a single usb cable to my PC.(win10).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-13 9:19 AM
​Now at work I get a different error message.
"Error in final launch sequence. Error in initializing ST_Link device, Reason: (4)
Everythings the same except at work I'm using a different board (STM32H747I-Eval), same MCU.