2024-03-11 3:14 AM
Hello,
i am trying to interface TI's ADS8910 (18bit SAR ADC) to an STM32F730 via normal SPI, since i am unsure whether QSPI will work.
I want to achieve the full 18 bit @1MSa, which is possible when working with 54MHz (/2 APB2 prescaler on the F730 which runs at full speed - 216MHz) and the ADC's zone 2 transfer.
The HAL implementation of dma transfer is way to slow between consecutive readouts and thus gets stuck "busy" and "locked" forever after the first readout.
Therefore i am currently trying to write everything myself.
My question is regarding the SPI CR2 register, bits 6 & 7 (RXNEIE and TXEIE):
Will the DMA requests, mentioned in Bits 0 & 1 (RXDMAEN and TXDMAEN) still be generated when the interrupts are masked?
I don't want my program to be interrupted more than neccessary.
the flow should be :
F7 gets an interrupt that signals that the ADC has finished conversion and is ready to send the new data.
SPI transfers 3x 8bits // or 2x 11bits (the ads 8910 needs at least 22 clocks)
DMA request is generated
DMA finishes transfer an generates an interrupt
Code handles data and SPI/DMA flags and enables/disables
Thanks in advance!
Michael
Solved! Go to Solution.
2024-03-11 6:10 AM
> Will the DMA requests, mentioned in Bits 0 & 1 (RXDMAEN and TXDMAEN) still be generated when the interrupts are masked?
Yes, DMA requests are handled regardless of interrupt configuration.
Consider capturing more than 1 sample per DMA buffer. The power of DMA is to capture many samples into a buffer and process them as a batch. This is more efficient than interrupting on every sample.
2024-03-11 6:10 AM
> Will the DMA requests, mentioned in Bits 0 & 1 (RXDMAEN and TXDMAEN) still be generated when the interrupts are masked?
Yes, DMA requests are handled regardless of interrupt configuration.
Consider capturing more than 1 sample per DMA buffer. The power of DMA is to capture many samples into a buffer and process them as a batch. This is more efficient than interrupting on every sample.
2024-03-11 6:34 AM
thanks for the quick answer!
I would like to, but i am unsure i can do it for the SPI to Memory part, the SPI on the F730 has only 1x 32bit FIFO each (one for RX and one for TX) and i need to clock and receive 22bits per sample. So i can't even buffer 2 Measurements in the FIFO.
2024-03-11 8:54 AM
I think TDK is not talking about the peripheral's FIFO, that's just an additional buffer between the SPI peripheral and the rest of the system.
So when starting DMA, assign it a memory buffer being able to hold more than one sample, change transfer length accordingly.
For my audio stuff using the I2S ( = SPI) I usually use DMA buffers big enough to give the MCU enough time for "working" with the data inbetween. Mostly several 100s of samples, but I don't do any real-time processing.
2024-03-12 1:39 AM
Thanks, i should definitely test that.
So far I've only been thinking about how i can process each sample before the next arrives, so that handling the raw data works in "real-time" and once i've stored a few hundred processed samples, i'd transfer them over to USB.
How do you deal with timed readouts in your applications? Do you leave dma enabled and only disable and re-enable SPI?
Or would it work to simply reload the NDTR only upon the interrupt? (with the dummy data, so that the Master starts clocking)
I have to read out every 1µs, which is signaled by an interrupt from the ADC.
I doubt I'd be fast enough for switching the stuff off and on if i'd work with the circular mode.
2024-03-12 5:07 AM
Isn't there any other way than to wait for this interrupt?
I actually don't know the SPI peripheral that well, so I can't tell if that ADC signal can somehow be "integrated" into the data transfer.
Maybe check the ADC datasheet again.
I usually use audio ADCs, clocked by the SAI or I2S (part of SPI) peripheral, so with the word clock (from stereo times often "LRCK") samples are read via the serial / bit clock, no need to wait for an interrupt.
For these transfers, DMA in circular mode is perfect, at high data rates with:
a) buffers big enough
b) working with DMA's half and complete interrupts (set flags to work on first or second half of the buffer)
c) and the best feature - if the STM32 type supports it (the F7 does so) - double buffer mode "DBM"
DBM was not yet supported by HAL when I started playing with that about 2 or 3 years ago.