RTC Problem with STM32F429ZIT6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-19 8:40 PM
With STm32F429ZIT6 the RTC battery used is 3.6V Ni-Cd and the RTC crystal used is 32.768khz. Initially, it works well for some days but after 1-2 months RTC date and time get reset to default value every time system is power reset.
Need help to resolve this ASAP.
Thanks in adcvance.
Solved! Go to Solution.
- Labels:
-
RTC
-
STM32F4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-25 11:04 PM
For primary designs with often recharge you don’t need bat, can be used supercap
For long time without power big capacity NiCd is ok (charge from 5V in your circuit) but with conv to 3V3 with low quiescient current around 100nA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-19 10:44 PM
Did you test the voltage of the Ni-Cd battery?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-19 11:19 PM
yes the voltage was 3.5 to 3.4 volts
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-20 12:04 AM
Hi. if you are sure that backup power is never lost, you MUST try to catch an unexpected sw behavior.
For example some cube mx version code generated put a 'magic' number in the first word of RTC backup.after setting time. At startup if magic word is no more present ,RTC would be initialized.
Few years ago we catch this after Cube MX /HAL upgrade.
Nor cube MX or HAL release note alert us that 1st RtC backup register is used for internal purpose...
Perhaps you use RTC backup register or sometimes unexpected write to it...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-20 6:15 AM
If it works for a few months, then stops working, sure seems like that is consistent with the battery losing voltage. Code doesn't execute differently after 1-2 months.
Note that if a battery is loaded, then you remove the load, the battery will recover some voltage and may appear as if it's fine, even though it's low and the voltage will drop when the load is reapplied.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-20 6:29 AM
Yes 3.4V is very discharged NiCd
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-21 7:52 PM
I tried replacing the battery but still, the problem persists. but if I replace the mico controller with a new one then the problem is solved. But that is not the required solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-21 11:16 PM
Also, what is the recommended battery for RTC of STM32F429?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-22 7:43 AM
If replacing the micro fixes it, the microcontroller is probably damaged. Keep in mind the max voltage you can put into VBAT and make sure you're under it at all times.
Any battery that has the proper voltage output range will work, such as a CR2032. NiCd batteries are very old/poor technology and aren't used much anymore.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-22 7:41 PM
@TDK which battery do you recommend for this uC? Does LIR2032 work?