cancel
Showing results for 
Search instead for 
Did you mean: 

RNG clock error on NUCLEO-L4A6ZG

JKo
Associate III

I am trying to use the RNG on the STM32L4A6ZG but every time I enable the RNG clock RNG_CR |= RNGEN the RNG_SR shows CEIS and CECS.

The AHB bus is at 80MHz and RNG_CLK is at 48MHz. I've tested with configuring the RNG_CLK to come from either the HSI48 or PLL48M2CLK by setting RCC_CCIPR CLK48SEL accordingly.

The RNG peripheral clock RCC_AHB2 |= RNGEN is also enabled.

PLL source is set to HSI16

PLL M = 1

PLL N = 20

PLL R = 4

PLL R output is enabled

SYSCLK source is set to PLLCLK

AHB PRESC is 1

PLLSAI1 N = 18

PLLSAI1 Q = 6

PLLSAI1 Q output is enabled

The problem seems to be related to either the HSI16 or the STM32L4A6ZG itself since I can configure and use the RNG on a custom board with an STM32L4A6RG but with a TCXO at 8MHz. PLL M = 2 and N = 80, PLLSAI1 N = 72, other values are the same as above.

I have also tried disabling the CED by writing 1 to RNG_CR.CED bit (with the RNGEN=0), but reading back the RNG_CR always shows CED=0.

Any ideas on what my problem could be? Something else I could try?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

> every time I enable the RNG clock RNG_CR |= RNGEN the RNG_SR shows CEIS and CECS.

And the other 3 status bits?

Can CEIS and CECS be cleared?

Is HSI16 running?

Read out and post content of all RCC and RNG registers.

JW

JKo
Associate III

Yes. HSI16 is running. The board and the USART peripherals wouldn't come up otherwise.

It did point me to look at the PLLSAI1 in the RCC_CR however and I found that was not enabled!

Turns out that on my other device which has USB enabled, the PLLSAI1 clock was enabled already but since I'm replacing the USB interface with a UART interface the PLLSAI1 clock wasn't enabled.

The HSI48 clock also required HSI48ON in the RCC_CRRCR if that source was selected.

Thanks.