RNG clock error on NUCLEO-L4A6ZG
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-04 11:04 AM
I am trying to use the RNG on the STM32L4A6ZG but every time I enable the RNG clock RNG_CR |= RNGEN the RNG_SR shows CEIS and CECS.
The AHB bus is at 80MHz and RNG_CLK is at 48MHz. I've tested with configuring the RNG_CLK to come from either the HSI48 or PLL48M2CLK by setting RCC_CCIPR CLK48SEL accordingly.
The RNG peripheral clock RCC_AHB2 |= RNGEN is also enabled.
PLL source is set to HSI16
PLL M = 1
PLL N = 20
PLL R = 4
PLL R output is enabled
SYSCLK source is set to PLLCLK
AHB PRESC is 1
PLLSAI1 N = 18
PLLSAI1 Q = 6
PLLSAI1 Q output is enabled
The problem seems to be related to either the HSI16 or the STM32L4A6ZG itself since I can configure and use the RNG on a custom board with an STM32L4A6RG but with a TCXO at 8MHz. PLL M = 2 and N = 80, PLLSAI1 N = 72, other values are the same as above.
I have also tried disabling the CED by writing 1 to RNG_CR.CED bit (with the RNGEN=0), but reading back the RNG_CR always shows CED=0.
Any ideas on what my problem could be? Something else I could try?
- Labels:
-
RCC
-
STM32L4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-04 3:02 PM
> every time I enable the RNG clock RNG_CR |= RNGEN the RNG_SR shows CEIS and CECS.
And the other 3 status bits?
Can CEIS and CECS be cleared?
Is HSI16 running?
Read out and post content of all RCC and RNG registers.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-04 5:32 PM
Yes. HSI16 is running. The board and the USART peripherals wouldn't come up otherwise.
It did point me to look at the PLLSAI1 in the RCC_CR however and I found that was not enabled!
Turns out that on my other device which has USB enabled, the PLLSAI1 clock was enabled already but since I'm replacing the USB interface with a UART interface the PLLSAI1 clock wasn't enabled.
The HSI48 clock also required HSI48ON in the RCC_CRRCR if that source was selected.
Thanks.