cancel
Showing results for 
Search instead for 
Did you mean: 

RM0456 Bookmarks repeat

waclawekjan_0-1695129324038.png

Some 'L4 RMs suffered/suffer from this, too (lazy to look up).

JW

1 ACCEPTED SOLUTION

Accepted Solutions

The bookmark issue is reported internally for all three reference manuals 

RM0351, RM0033: Internal ticket number 133462

RM0456: Internal ticket number 156018

Thank you!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Sarra.S
ST Employee

Hello @waclawek.jan

Thank you for bringing up this issue! I can confirm the same issue in RM0351

Edit : also RM0033

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The bookmark issue is reported internally for all three reference manuals 

RM0351, RM0033: Internal ticket number 133462

RM0456: Internal ticket number 156018

Thank you!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, @Sarra.S .

Jan

Hi @Sarra.S ,

This thing is like a plague (pdf software issue I guess). While the new versions of RM0351 ('L4) and RM0456 ('U5) are now OK, the brand new RM0316 ('F303) suffers now from the problem.

waclawekjan_0-1710427557924.png

 

JW

Hello Jan, thank you for spotting this! 

I consolidated all the previous tickets when reporting this ongoing problem (Ticket 176177)

Thank you! 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, @Sarra.S .

JW