cancel
Showing results for 
Search instead for 
Did you mean: 

RM0455 STM32H7A/B: Reset state of SYSCFG_PMCR incorrect?

Andreas Bolsch
Lead II

RM0455, rev. 6, says reset state of SYSCFG_PMCR is 0x0F00 0000.

But STM32H7A3ZIT6Q, rev. Z, shows 0x0300 0000 instead, i.e. PC2 and PC3 switches closed. not open. Does this depend on package as PC2 and PC3 are not bonded out for this particular package?

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Andreas Bolsch (Community Member)​ ,

In fact, the value depends on the packages.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

8 REPLIES 8
TDK
Guru

FWIW, on my STM32H7B3I-DK board, the reset value is 0, barring any bugs in the SVD file. That chip has all 8 pins present.

If you feel a post has answered your question, please click "Accept as Solution".

Hm, for STM32H7B3LIH6Q, rev. Z, on STM32H7B3I-DK I see reset value 0x0F00 0000 ...

That you observed 0 might be due to disabled clock, i.e. SYSCFGEN in RCC_APB4ENR not being set.

Hello @Andreas Bolsch (Community Member)​ ,

In fact, the value depends on the packages.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Makes sense, indeed, although at first somewhat unexpected ;)

You're probably right, that slipped my mind.

If you feel a post has answered your question, please click "Accept as Solution".

Shouldn't that still be properly documented?

JW

Imen.D
ST Employee

Hi @Community member​ ,

I raised the same feedback internally :)

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks, Imen.

Jan