cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440 Rev. 2: Number of significant bits in FLASH_WRPxxR apparently wrong.

Andreas Bolsch
Lead II

RM says for both Cat. 2 and Cat. 3 devices all WRPxxR have 7 significant bits, and production values for option bytes starting at 0x1FFF7818 are 0xFF*0*0FFFF.

This suggests that bit 7 in WRP_xxR reads '0''.

However, actual G431RB has only 6 significant bits (checked by toggling) and production value is 0xFF*C*0FFFF (supporting 6 bits). Whereas G474RE has indeed 7 and production value is 0xFF*8*0FFFF.

So, bit 6 and 7 for Cat. 2 always read as '1' and for Cat. 3 bit 7 always read as '1'?

Now what about Cat. 3 with only 128 kByte or 256 kByte? Still 7 bits and 0xFF*8*0FFFF ?

BTW: There is a similar discrepancy in RM 0444 and 0454: G03x have only 5 significant bits, not 6. But there the unused bits read '0'.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @Andreas Bolsch​ ,

This is already updated and corrected in new RM0440 (draft) that will be available soon on ST web site.

Thank you for your contribution and highlighting this.

So, keep an eye out for the next release!

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen