cancel
Showing results for 
Search instead for 
Did you mean: 

RM0432 - HSITRIM default value might be wrong?

irinanita
Associate

In the reference manual for STM32L4+ (RM0432), it states that the default value for HSITRIM[6:0] is 16, which seems to be the default for MCUs that have 5 bits allocated for the trimming value, not 7. The reset value is correct, but I suppose it should be also stated in the description as 64 (0x40), instead of 16 (0x10).

STM32L4-HSITRIM.png

 

3 REPLIES 3
Issamos
Lead II

Hello @irinanita 

It seems to be a typo in the RM0432. Could you please @STOne-32 ، @Imen.D confirm it and report it. 

Best regards.

II

Hello @irinanita and welcome to the Community :)

Let me first welcome you to the STM32 Community and thank you for reporting this issue.

Thank you @Issamos for bringing this post to our attention.

I confirm the mistake in description of HSITRIM[6:0]. The default value should be 64 (as written in default reset value of register: 0x40 = 64).

An internal ticket (ID160618) is submitted in order to correct the RM0432 in the coming releases.
PS: ID 160618 is an internal tracking number and is not accessible or usable by customers.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks @Imen.D