cancel
Showing results for 
Search instead for 
Did you mean: 

CAN communication

rohitkumarkv07
Associate III

I want to establish can communication on CAN1 in which message being transmitted ,after every 5 m,/s. Below is my main.c and mcu.c .

This is mcu.c file.

 

 

#include "Mcu.h"
#include "Mcu_Config.h"
#include "Mcu_Internal.h"
#include "Mcu_RegTypes.h"
#include "stm32f407xx.h"

Mcu_ConfigType* Mcu_pConfigPtr = NULL_PTR;

#define RCC_CRREG  ((uint32*)RCCREG_BASE)

static FUNC(void, MCU_CODE) Mcu_Pwr_Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_Flash_Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AllPeriphralReset(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB1Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB2Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_AHB3Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_APB1Init(VAR( void, AUTOMATIC));
static FUNC(void, MCU_CODE) Mcu_APB2Init(VAR( void, AUTOMATIC));

static FUNC(void, MCU_CODE) Mcu_Pwr_Init(VAR( void, AUTOMATIC))
{
	PwrConfigType* LpPwrConfigPtr;
	PWR_RegTypedef* LpPWR_Reg = PWR_REGADDRESS;

	LpPwrConfigPtr = Mcu_pConfigPtr->PWRConfgSet;
#if(MCU_VOS_SCALE_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.VOS;
#endif
#if(MCU_FPDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.FPDS;
#endif
#if(MCU_DBP_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.DBP;
#endif
#if(MCU_PLS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PLS;
#endif
#if(MCU_PVDE_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PVDE;
#endif
#if(MCU_PDDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.PDDS;
#endif
#if(MCU_LPDS_USED == STD_ON)
	LpPWR_Reg->CR |= LpPwrConfigPtr->PwrCRConfgVal.LPDS;
#endif

#if(MCU_BRE_USED == STD_ON)
	LpPWR_Reg->CSR |= LpPwrConfigPtr->PwrCSRConfgVal.BRE;
#endif
#if(MCU_EWUP_USED == STD_ON)
	LpPWR_Reg->CSR |= LpPwrConfigPtr->PwrCSRConfgVal.EWUP;
#endif

}

static FUNC(void, MCU_CODE) Mcu_Flash_Init(VAR( void, AUTOMATIC))
{
	FLASHConfigType* LpFlashconfigPtr;
	FLASH_RegTypedef* LpFLASH_Reg = FLASH_REGADDRESS;
	LpFlashconfigPtr = Mcu_pConfigPtr->FlashConfgSet;

#if(MCU_DCRST_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.DCRST;
#endif
#if(MCU_ICRST_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.ICRST;
#endif
#if(MCU_LATENCY_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.LATENCY;
#endif
#if(MCU_DCEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.DCEN;
#endif
#if(MCU_ICEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.ICEN;
#endif
#if(MCU_PRFTEN_USED == STD_ON)
	LpFLASH_Reg->ACR |= LpFlashconfigPtr->FLASHACRConfgVal.PRFTEN;
#endif

}
static FUNC(void, MCU_CODE) Mcu_AllPeriphralReset(VAR( void, AUTOMATIC))
{
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	/*Reset the MCU Peripherals */
	LpRCC_Reg->AHB1RSTR =(uint32)(RCC_AHB1RSTR_RESET);
	LpRCC_Reg->AHB1RSTR =(uint32)(0x00000000);
	LpRCC_Reg->AHB2RSTR =(uint32)(RCC_AHB2RSTR_RESET);
	LpRCC_Reg->AHB2RSTR =(uint32)(0x00000000);
	LpRCC_Reg->AHB3RSTR =(uint32)(RCC_AHB3RSTR_RESET);
	LpRCC_Reg->AHB3RSTR =(uint32)(0x00000000);
	LpRCC_Reg->APB1RSTR =(uint32)(RCC_APB1RSTR_RESET);
	LpRCC_Reg->APB1RSTR =(uint32)(0x00000000);
	LpRCC_Reg->APB2RSTR =(uint32)(RCC_APB2RSTR_RESET);
	LpRCC_Reg->APB2RSTR =(uint32)(0x00000000);
	/*Reset the MCU Peripherals */
}
static FUNC(void, MCU_CODE) Mcu_AHB1Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	/*McuAHB1ENRConfgVal*/
#ifdef MCU_USB_OTG_USED
#if(OTGHSULPIEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.OTGHSULPIEN;
#endif
#if(OTGHSEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.OTGHSEN;
#endif
#endif

#ifdef MCU_ETHMAC_USED
#if(ETHMACPTPEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACPTPEN;
#endif
#if(ETHMACRXEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACRXEN;
#endif
#if(ETHMACTXEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACTXEN;
#endif
#if(ETHMACEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.ETHMACEN;
#endif
#endif

#ifdef MCU_DMA_USED
#if(DMA2EN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.DMA2EN;
#endif
#if(DMA1EN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.DMA1EN;
#endif
#endif

#ifdef MCU_CCM_DATA_RAM_USED
#if(CCMDATARAMEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.CCMDATARAMEN;
#endif
#endif

#ifdef MCU_BKP_SRAM_USED
#if(BKPSRAMEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.BKPSRAMEN;
#endif
#endif

#ifdef MCU_CRC_USED
#if(CRCEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.CRCEN;
#endif
#endif

#ifdef MCU_GPIO_USED
#if(GPIOIEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOIEN;
#endif
#if(GPIOHEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOHEN;
#endif
#if(GPIOGEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOGEN;
#endif
#if(GPIOFEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOFEN;
#endif
#if(GPIOEEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOEEN;
#endif

#if(GPIODEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIODEN;
#endif

#if(GPIOCEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOCEN;
#endif
#if(GPIOBEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOBEN;
#endif
#if(GPIOAEN_USED == STD_ON)
	LpRCC_Reg->AHB1ENR |= LpMcuClockConfigPtr->McuAHB1ENRConfgVal.GPIOAEN;
#endif
#endif
}
static FUNC(void, MCU_CODE) Mcu_AHB2Init(VAR( void, AUTOMATIC))
{
	//McuClockConfigType* LpMcuClockConfigPtr;

	//RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	//LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	/*McuAHB2ENRConfgVal*/
#if(OTGFSEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.OTGFSEN;
#endif
#if(RNGEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.RNGEN;
#endif
#if(HASHEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.HASHEN;
#endif
#if(CRYPEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.CRYPEN;
#endif
#if(DCMIEN_USED == STD_ON)
	LpRCC_Reg->AHB2ENR |= LpMcuClockConfigPtr->McuAHB2ENRConfgVal.DCMIEN;
#endif


}
static FUNC(void, MCU_CODE) Mcu_AHB3Init(VAR( void, AUTOMATIC))
{
	//McuClockConfigType* LpMcuClockConfigPtr;

	//RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	//LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;

	/*McuAHB3ENRConfgVal*/
#if(DCMIEN_USED == STD_ON)
	LpRCC_Reg->AHB3ENR |= LpMcuClockConfigPtr->McuAHB3ENRConfgVal.FSMCEN;
#endif
}
static FUNC(void, MCU_CODE) Mcu_APB1Init(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;

	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


	/*McuAPB1ENRConfgVal*/
#ifdef MCU_DAC_USED
#if(DACEN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.DACEN;
#endif
#endif
#ifdef MCU_PWR_USED
#if(PWREN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.PWREN;
#endif
#endif
#ifdef MCU_CAN_USED
#if(CAN2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.CAN2EN;
#endif
#if(CAN1EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.CAN1EN;
#endif
#endif

#ifdef MCU_I2C_USED
#if(I2C3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C3EN;
#endif
#if(I2C2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C2EN;
#endif
#if(I2C1EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.I2C1EN;
#endif
#endif
#ifdef MCU_UART_USED
#if(UART5EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART5EN;
#endif
#if(UART4EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART4EN;
#endif
#endif
#ifdef MCU_USART_USED
#if(USART3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.USART3EN;
#endif
#if(USART2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.USART2EN;
#endif
#endif
#ifdef MCU_SPI_USED
#if(SPI3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.SPI3EN;
#endif
#if(SPI2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.SPI2EN;
#endif
#endif
#if(WWDGEN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.WWDGEN;
#endif
#ifdef MCU_TIM_USED
#if(TIM14EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.UART4EN;
#endif
#if(TIM13EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM13EN;
#endif
#if(TIM12EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM12EN;
#endif
#if(TIM7EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM7EN;
#endif
#if(TIM6EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM6EN;
#endif
#if(TIM5EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM5EN;
#endif
#if(TIM4EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM4EN;
#endif
#if(TIM3EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM3EN;
#endif
#if(TIM2EN_USED == STD_ON)
	LpRCC_Reg->APB1ENR |= LpMcuClockConfigPtr->McuAPB1ENRConfgVal.TIM2EN;
#endif
#endif

}
static FUNC(void, MCU_CODE) Mcu_APB2Init(VAR( void, AUTOMATIC))
{
	//McuClockConfigType* LpMcuClockConfigPtr;

	//RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

	//LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


	/*McuAPB2ENRConfgVal*/
#ifdef MCU_TIM_USED
#if(TIM11EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM11EN;
#endif
#if(TIM10EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM10EN;
#endif
#if(TIM9EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM9EN;
#endif
#endif
#if(SYSCFGEN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SYSCFGEN;
#endif
#if(SPI1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SPI1EN;
#endif
#if(SPI1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.SDIOEN;
#endif
#ifdef MCU_ADC_USED
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC3EN;
#endif
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC2EN;
#endif
#if(ADC3EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.ADC1EN;
#endif
#endif
#ifdef MCU_USART_USED
#if(USART6EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.USART6EN;
#endif
#if(USART5EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.USART1EN;
#endif
#endif
#ifdef MCU_TIM_USED
#if(TIM8EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM8EN;
#endif
#if(TIM1EN_USED == STD_ON)
	LpRCC_Reg->APB2ENR |= LpMcuClockConfigPtr->McuAPB2ENRConfgVal.TIM1EN;
#endif
#endif
}

/*
 * Enable Peripherals
 * 	Mcu_AHB1Init();
 * 	Mcu_AHB2Init();
 * 	Mcu_AHB3Init();
 * 	Mcu_APB1Init();
 * 	Mcu_APB2Init(); */
FUNC(void, MCU_CODE) Mcu_Init( Mcu_ConfigType* pConfigPtr)
{
	Mcu_pConfigPtr = pConfigPtr;

	Mcu_AllPeriphralReset();
	Mcu_Pwr_Init();
	Mcu_Flash_Init();
	Mcu_AHB1Init();
	Mcu_AHB2Init();
	Mcu_AHB3Init();
	Mcu_APB1Init();
	Mcu_APB2Init();
}
/*
 * Enable HSE or HSI
 * Configure PLLCFGR
 * Configure CFGR (if applicable)
 * Configuring PLL */
FUNC( Std_ReturnType, MCU_CODE) Mcu_InitClock( VAR( uint8, AUTOMATIC) ClockSetting)
{
	McuClockConfigType* LpMcuClockConfigPtr;
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;
	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSITRIM;
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSION;
	/*HSI TRIM -> Set to Default value -->to be Implemented*/

#if(MCU_HSE_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.HSEON;
	/* Wait for HSEON ready*/
	while (!(LpRCC_Reg->CR & (1 << 17)));
#if(MCU_PLL_USED == STD_OFF)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.SW;
#endif
#endif
	/* Configure AHB PreScaler->HCLK,
	 * APB1 Prescaler->PCLK1,
	 * APB2 Prescaler->PCLK2*/
	/*Clear SW, HPRE, PPRE1, and PPRE2 bits*/
	RCC->CFGR &= ~(RCC_CFGR_HPRE | RCC_CFGR_PPRE1 | RCC_CFGR_PPRE2);
	/*RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
	RCC->CFGR |= RCC_CFGR_PPRE1_DIV8;
	RCC->CFGR |= RCC_CFGR_PPRE2_DIV2;*/


	/* Configure AHB prescaler*/
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.HPRE;
	/* Configure APB1 prescaler*/
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.PPRE1;
	/*Configure APB2 prescaler*/
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.PPRE2;

	LpRCC_Reg->PLLCFGR &= 0xFFFF8000;
#if(MCU_PLL_USED == STD_ON)
	LpRCC_Reg->PLLCFGR |=LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLM;
	LpRCC_Reg->PLLCFGR |=LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLN;
	LpRCC_Reg->PLLCFGR |=LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLP;
	LpRCC_Reg->PLLCFGR |=LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLSRC;
	LpRCC_Reg->PLLCFGR |=LpMcuClockConfigPtr->McuPLLCFGRConfgVal.PLLQ;
#endif

#if(MCU_MCO2_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO2;
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO2PRE;
#endif
#if(MCU_MCO1_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO1;
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.MCO1PRE;
#endif
#if(MCU_I2SSRC_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.I2SSRC;
#endif
#if(MCU_RTC_USED == STD_ON)
	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.RTCPRE;
#endif



#if 0
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.PLLI2SRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.PLLRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.HSERDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.HSIRDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.LSERDYIE;
#endif
#if(MCU_RTC_PREHSE_1_USED == STD_ON)
	LpRCC_Reg->CIR|=LpMcuClockConfigPtr->McuCIRConfgVal.LSIRDYIE;
#endif
#endif

#if(MCU_PLL_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.PLLON;
#endif

#if(MCU_PLLI2S_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.PLLI2SON;
#endif

#if 0
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.BDRST;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.RTCEN;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.RTCSEL;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.LSEBYP;
	LpRCC_Reg->BDCR = LpMcuClockConfigPtr->McuBDCRConfgVal.LSEON;
	LpRCC_Reg->CSR = LpMcuClockConfigPtr->McuCSRConfgVal.LSION;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.SSCGEN;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.SPREADSEL;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.INCSTEP;
	LpRCC_Reg->SSCGR = LpMcuClockConfigPtr->McuSSCGRConfgVal.MODPER;
	LpRCC_Reg->PLLI2SCFGR = LpMcuClockConfigPtr->McuPLLI2SCFGRConfgVal.PLLI2SR;
	LpRCC_Reg->PLLI2SCFGR = LpMcuClockConfigPtr->McuPLLI2SCFGRConfgVal.PLLI2SN;
#endif
	return E_OK;
}

/* Get Status of PLL after turning PLL to ON in CR */
FUNC( Std_ReturnType, MCU_CODE) Mcu_GetPllStatus(VAR( void, AUTOMATIC))
{
	static Mcu_PllStatusType status = MCU_PLL_STATUS_UNDEFINED;
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;

#if(MCU_PLL_USED == STD_OFF)
	status = MCU_PLL_LOCKED;
#else
	// Check if PLL is ready
	if(LpRCC_Reg->CR & (1<<25)) {
		status = MCU_PLL_LOCKED;
	} else {
		status = MCU_PLL_UNLOCKED;
	}
	return status;
#endif
}

/* Distribute HSI/ HSE/ PLL via CFGR->SW1_SW0*/
FUNC( Std_ReturnType, MCU_CODE) Mcu_DistributePllClock(VAR( void, AUTOMATIC))
{
	McuClockConfigType* LpMcuClockConfigPtr;
	RCC_RegTypedef* LpRCC_Reg = RCC_REGADDRESS;
	LpMcuClockConfigPtr = Mcu_pConfigPtr->McuClockConfgSet;


#if(MCU_CSS_USED == STD_ON)
	LpRCC_Reg->CR |= LpMcuClockConfigPtr->McuCRConfgVal.CSSON;
#endif

	LpRCC_Reg->CFGR |= LpMcuClockConfigPtr->McuCFGRConfgVal.SW;

	return E_OK;
}






 

 

this is main.c file.

 

 

#include "Mcu.h"
#include "stm32f4xx.h"
#include "Mcu_RegTypes.h"
#include "Mcu_InternalTypes.h"

#define LED_PIN 12  // Assuming the LED is connected to GPIO Port D, Pin 12

/*void delay(uint32_t milliseconds)
{
	// Assuming the system clock is running at 16MHz
	uint32_t ticks = milliseconds * 16000;
	while (ticks--);
}
*/
void TIM2_IRQHandler()
{
	if (TIM2->SR & TIM_SR_UIF) // Check if update interrupt flag is set
	{
		TIM2->SR &= ~TIM_SR_UIF; // Clear the update interrupt flag

		// Toggle pin 12
		GPIOD->ODR ^= GPIO_ODR_OD12;
	}
}

int main()
{
	Mcu_Init(&Mcu_ConfigSet[0]);
	Mcu_InitClock(0);
	while (MCU_PLL_LOCKED != Mcu_GetPllStatus());
	Mcu_DistributePllClock();

	// Configure PD12 as output
	GPIOD->MODER |= GPIO_MODER_MODER12_0;

	// Configure output type as push-pull
	GPIOD->OTYPER &= ~GPIO_OTYPER_OT_12; // Push-pull output

	// Enable TIM2 clock
	//RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
	// Already enable through config.c

	// Set TIM2 prescaler to get 1ms ticks assuming 16MHz clock
	TIM2->PSC = 16000 - 1;

	// Set TIM2 auto-reload value to get a 5s period
	TIM2->ARR = 5000 - 1;

	// Enable TIM2 update interrupt
	TIM2->DIER |= TIM_DIER_UIE;

	// Set TIM2 priority
	NVIC_SetPriority(28, 0x01);

	// Enable TIM2 interrupt in NVIC
	NVIC_EnableIRQ(28);

	NVIC_SetVector(28,(uint32)&TIM2_IRQHandler);

	// Start TIM2
	TIM2->CR1 |= TIM_CR1_CEN;

	while (1)
	{
		// Main program loop, no need for delay here
	}
}

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mƎALLEm
ST Employee

Well, so what is the problem? and I don't see any CAN code in your main!

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Don't use the RMW form here

TIM2->SR &= ~TIM_SR_UIF; // Clear the update interrupt flag

Just write the mask, it's safer and lacks secondary effects

TIM2->SR = ~TIM_SR_UIF; // Clear the update interrupt flag

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..