2023-10-29 01:04 PM - edited 2023-10-29 01:08 PM
Hi!
Noticed a typo in the system configuration controller (SYSCFG) register map in both reference manuals RM0399 (Rev 4) and RM0433 (Rev 8).
The SYSCFG_CCCR register is at two different offsets (0x28 and 0x2C) and SYSCFG_PWRCR is missing. I think, SYSCFG_CCCR should be at offset 0x28 and SYSCFG_PWRCR at 0x2C.
2023-10-30 12:04 AM - edited 2023-10-30 12:15 AM
Hello @krotti42 and welcome to the community 🙂,
Thank you for bringing this issue to our attention.
I confirm that SYSCFG_PWRCR register is missing and SYSCFG_CCCR register is mentioned twice in SYSCFG register map and reset values table.
I reported internally this typo.
Internal ticket number: 165221 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.