RF feature of STM32W108CB microcontroller
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-07 6:34 AM
Posted on November 07, 2013 at 15:34
Hello,
I want to establish a simple point to point RF communication using STM32w108CB microcontroller. I used the STM32w RF control kit to understand how to use the RF feature. I find the simpleMAC library file for example has the all the necessary functions to establish the RF communication. Now I want to use the STM32w108CB microcontroller to perform the similar task. I built the similar antenna circuit as of the evaluation board and also I copied the simpleMAC library file into my project. But I could not program the RF to transmit data. It gives me lot of errors. I have already programmed the STM32w108CB to acquire data from a sensor and store it in DMA memory. Now I need to transfer this data to a receiver using RF. My question is is there any library that I need to include in the project file to use the RF feature? I modified the sample code given for the evaluation board to allow the SPI to acquire data and transmit the data wirelessly from one board to another evaluation board. I programmed one board as transmitter and other as a receiver. The program works perfect and I view all the data in a hyperterminal window. Since all the library features and files are already given for the board, I could easily establish the RF communication. But how do I establish the similar communication using STM32W108CB? What are all the library files that I need to add to use the RF feature of the microcontroller. Because details of all other peripherals are given in the STM32w108xx_StdPeriph_Driver. Regards, Kavita #rf-interface #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-11 4:35 AM
Posted on November 11, 2013 at 13:35
Hi Kavita,
It seems that the STM32W108xx_HAL_Driveris missed, right?
In fact, to use the RF features, you have to include the binary library (example: simplemac-library.a) and the folder STM32W108xx_HAL_Driver.
In the SimpleMAC package there are some examples with the right environment that could be used.
-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-13 3:19 AM
Posted on November 13, 2013 at 12:19
Hi Mayla,
Thanks for the reply. I have tried adding the HAL driver and simpleMAC library to the project folder but still it gives me errors. When I add the HAL library, it asks me to choose the development board type (MB950. MB951...). How do I program the RF feature in my board?