cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427 HardFault

jjens2
Associate
Posted on November 13, 2013 at 14:05

Hello

The original program was tested on STM32F407ZG MCU, but I need to have it running on a STM32F427ZI.

On the 407 the code was running fine, but when I start the debugger with the new modified program it stops at

''HardFault_Hadler() at stm32f4xx_it.c:64 0x800042A''

''<signal handler called> () at 0xfffffff9''

''__libc_init_array() at 0x80017ce''

I have reduced the code to a minimum (only initialising rcc and gpio) and to toggle an LED, but still getting this error.

I am using Atollic Truestudio Pro 4.2.0 and have already changed the ID file to ''STM32F427ZI.Id'', changed the compiler settings and modified startup file and stm32f4xx.h to match the new contoller.

Any idea what might cause this?

Jörn
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
frankmeyer9
Associate II
Posted on November 13, 2013 at 14:27

''<signal handler called> () at 0xfffffff9''

 

''__libc_init_array() at 0x80017ce''

 

Perhaps something is wrong with your project settings.

Interpreting 0x80017CE as address of function __libc_init_array(), it seems ''odd to be even''. That means, I would expect an odd address, to mark it as thumb routine.

Accidently linked against ARM code ?