2023-09-22 4:01 AM
Currently we are using STM32F4 & STM32H7 controller with inbuilt ethernet. We are looking to add a profinet interface in our device without using additional external hardware.
Please can you share references or documents how can we integrate Profinet stack on STM32F4 & STM32H7 hardware. Also share us the official and available Profinet stacks which we can use without using extra hardware on STM32F4 & STM32H7 .
Please share the references and guides, It will be helpful.
2023-09-22 4:11 AM
Hello @PKote.2
You can use the Port PROFINET wish is compatible with the STM32F4 et STM32F7.
best regards.
II
2023-09-25 3:23 AM - edited 2023-09-25 3:30 AM
Hi Issamos,
we are using STM32H7 controller as well. Is port PROFINET stack supports STM32H7 also.
Best Regards,
Pavan Kote
2023-09-25 3:56 AM
Hello @PKote.2
The stack I've shared above is compatible only with STM32F4 and F7 series. I don't have any information about the H7 series.
Best regards.
II
2023-09-25 10:10 AM
Hi @PKote.2
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2023-09-26 12:41 AM