cancel
Showing results for 
Search instead for 
Did you mean: 

Request for info on Profinet Stack Availability or Third party stacks supported by STM32H7-Profinet

PKote.2
Associate II

Currently we are using STM32F4 & STM32H7 controller with inbuilt ethernet. We are looking to add a profinet interface in our device without using additional external hardware.

Please can you share references or documents how can we integrate Profinet stack on STM32F4 & STM32H7 hardware. Also share us the official and available Profinet stacks which we can use without using extra hardware on STM32F4 & STM32H7 .

Please share the references and guides, It will be helpful.

5 REPLIES 5
Issamos
Lead II

Hello @PKote.2 

You can use the Port PROFINET wish is compatible with the STM32F4 et STM32F7.

best regards.

II

Hi Issamos,

we are using STM32H7 controller as well. Is port PROFINET stack supports STM32H7 also.

Best Regards,

Pavan Kote

Hello @PKote.2 

The stack I've shared above is compatible only with STM32F4 and F7 series. I don't have any information about the H7 series.

Best regards.

II

Billy OWEN
ST Employee

Hi @PKote.2 

 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

 

Regards,

Billy

PKote.2
Associate II

Hi Billy,

That will be very helpful.

Best Regards,

Pavan Kote