2024-09-25 06:10 AM
Hi,
I am looking for the STM32H series part with more GPIOs and Timers than STM32H753ZI. Can you please suggest me some of the options in H series?
Below is my requirement
GPIO | SPI | I2C | UART | Timer | CAN | Internal ADC Channel |
60 | 5 | 2 | 2 | 16 | 2 | 17 |
Solved! Go to Solution.
2024-09-25 08:35 AM - edited 2024-09-25 08:44 AM
Hello @DJ7 ,
When you say STM32H, it could be STM32H5 or STM32H7.
Anyway, you can refer to the datasheet. For example in case of STM32H742xI/G /STM32H743x / STM32H753 Table 2: it shows all the instances available on the MCU.
For example for the GPIOs number, it depends on the package:
SPI/I2C/USART instances:
But becarefull, you need to check if all these instances could be used in parallel.
2024-09-25 06:16 AM - edited 2024-09-25 06:20 AM
Hello @DJ7 and welcome to the ST Community.
For such a use case, I suggest you use the STM32-MCU-FINDER this tool where you could define what you want exactly, and the tool will give you all available options.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-25 06:16 AM
2024-09-25 08:35 AM - edited 2024-09-25 08:44 AM
Hello @DJ7 ,
When you say STM32H, it could be STM32H5 or STM32H7.
Anyway, you can refer to the datasheet. For example in case of STM32H742xI/G /STM32H743x / STM32H753 Table 2: it shows all the instances available on the MCU.
For example for the GPIOs number, it depends on the package:
SPI/I2C/USART instances:
But becarefull, you need to check if all these instances could be used in parallel.