cancel
Showing results for 
Search instead for 
Did you mean: 

Replacement for STM32H753ZI

DJ7
Associate

Hi,

 

I am looking for the STM32H series part with more GPIOs and Timers than STM32H753ZI. Can you please suggest me some of the options in H series?

Below is my requirement

 

GPIOSPII2CUARTTimerCANInternal ADC Channel
6052216217
3 REPLIES 3
STTwo-32
ST Employee

Hello @DJ7 and welcome to the ST Community.

For such a use case, I suggest you use the STM32-MCU-FINDER this tool where you could define what you want exactly, and the tool will give you all available options.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

SofLit
ST Employee

Hello @DJ7 ,

When you say STM32H, it could be STM32H5 or STM32H7.

Anyway, you can refer to the datasheet. For example in case of STM32H742xI/G /STM32H743x / STM32H753 Table 2: it shows all the instances available on the MCU. 

For example for the GPIOs number, it depends on the package:

SofLit_0-1727278239695.png

SPI/I2C/USART instances:

SofLit_1-1727278411428.png

But becarefull, you need to check if all these instances could be used in parallel.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.