cancel
Showing results for 
Search instead for 
Did you mean: 

Remounting Sd Card

DeepakY
Associate II

I am working with stm32h750xb.  i want to mount and write data at different time interval

i am using fatfs and SDMMC  


If i mount it in main and try to write in loop it is not working it showing error

            so i did both in loop i was able to write and read. but i can do it only once , if i unmount and try to mount again its showing error 

So i want to know how to remount after unmounting 

and also why i am not able to write if i mount in main and write in loop

 

   

2 REPLIES 2
Andrew Neil
Super User

@DeepakY wrote:

its showing error 


What is showing error?

What error(s), exactly, is it showing?

What debugging have you done to find the reason for the error?

Give full hardware and software details.

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
DeepakY
Associate II

thank you
i found the problem i did not giving delay after unmounting 

i have one more problem

whenever i turn on stm32 the memory card will not get initialized at beginning i need to press reset 3 to 4 times sometimes it does not get initialized after trying for long period also

here is the code 

STATUS stat = RES_OK;

stat= disk_initialize(0);

HAL_Delay(500);

printDriveStatus(stat);

 

while (f_mount(&SDFatFS, (TCHAR const*)SDPath, 1) != FR_OK)

{

 

}