cancel
Showing results for 
Search instead for 
Did you mean: 

References to TIM5 in RM0091

There is no TIM5 in the 'F0.

Textual search for TIM5 in RM0091 rev.9 reveals it occurs twice:

  • in Internal clock source (CK_INT) subchapter of TIM15/16/17 chapter; this is a typo and it ought to be TIM15 (because TIM16/17 don't have the slave-mode controller this sentence refers to)
  • in the Index, as TIM5_OR, this ought to be TIM14_OR

ST, please correct.

Thanks,

JW

1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi Jan,

these typos are tracked internally to be fixed in new version of RM0091.

Thanks

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Uwe Bonnes
Principal III

RM0090 is about F4, probably you mean RM0091.

Yes, thanks. I've corrected the post and title.

JW

Amel NASRI
ST Employee

Hi Jan,

these typos are tracked internally to be fixed in new version of RM0091.

Thanks

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, Amel.

Jan