2022-01-31 01:00 AM
hey there
I have a customized board with STM32F030K6T6 on it and a 11.0592MHz crystal for HSE. the thing is my code does not run through and when I try to debug it, I can see it sticks in SystemClock_Config(), more specifically, in HAL_RCC_OscConfig() and when I trace it even more I get to __HAL_RCC_HSE_CONFIG() which seems like is responsible for bit setting and stuff...
any ways I have no Idea why this happens and though I think crystal is just fine(the reason is that I have tested my code in other boards and it was OK! therefore I dont think the problem is my code, it should be hardware somehow but I dont know what it could be?)
HELP!
Solved! Go to Solution.
2022-02-01 01:26 AM
The current version of STM32CubeMX generates a while trap in USER CODE NonMaskableInt_IRQn 1:
void NMI_Handler(void)
{
/* USER CODE BEGIN NonMaskableInt_IRQn 0 */
/* USER CODE END NonMaskableInt_IRQn 0 */
HAL_RCC_NMI_IRQHandler();
/* USER CODE BEGIN NonMaskableInt_IRQn 1 */
while (1)
{
}
/* USER CODE END NonMaskableInt_IRQn 1 */
}
Good luck!
Regards
/Peter
2022-01-31 01:37 AM
I guess that crystal is not properly soldered to the board, as I push it to the board, my code runs, and as soon as I leave it, it stops
2022-01-31 02:04 AM
Yes, that could well be a problem.
There are, however, ways to catch the issue, because it could also occur during operation (e.g. broken internal bond wires of the crystal): the CSS (Clock Security System) is designed to switch over to the HSI in the event of a failure of the HSE and also to report it via NMI. Details can be found in RM0360, section 7.2.7.
Regards
/Peter
2022-01-31 09:21 PM
thanks @Peter BENSCH
is there a way to enable CSS in CubeMX? I mean I have enable it in Clock configuration panel, but I dont think this helped... it still has problem sticking in RCC... should I do something in void NMI_Handler(void) interrupt?
regards
2022-02-01 12:02 AM
Well, if you don't change NMI_Handler() accordingly, the function gets stuck in while(1).
The description for HAL_RCC_EnableCSS(), inserted in SystemClock_Config(), says:
If a failure is detected on the HSE oscillator clock, this oscillator is automatically disabled and an interrupt is generated to inform the software about the failure (Clock Security System Interrupt, CSSI), allowing the MCU to perform rescue operations. The CSSI is linked to the Cortex-M0 NMI (Non-Maskable Interrupt) exception vector.
So you'll get a top priority information that HSE has failed, but of course only you know what to do then.
Regards
/Peter
2022-02-01 12:53 AM
"Well, if you don't change NMI_Handler() accordingly, the function gets stuck in while(1)."
I dont see any while(1) here is the generated code
void NMI_Handler(void)
{
/* USER CODE BEGIN NonMaskableInt_IRQn 0 */
/* USER CODE END NonMaskableInt_IRQn 0 */
HAL_RCC_NMI_IRQHandler();
/* USER CODE BEGIN NonMaskableInt_IRQn 1 */
/* USER CODE END NonMaskableInt_IRQn 1 */
}
let me ask my question in a different way:
1-if I enable CSS in CubeMX, even if HSE fails, I have the security of switching to HSI, right? nothing to do further?
2-of curse if HSE fails, it will inform me through NMI_Handler()(above code), where I can insert my customized code. assuming HSE has failed and MCU has switched to HSI. and now for example I want to inform this using USART. does UART work now? we all know that UART needs a very accurate clock. are you saying switching to HSI, manages UART?
thanks for you helpful and informative replies🙏
Regards
2022-02-01 01:26 AM
The current version of STM32CubeMX generates a while trap in USER CODE NonMaskableInt_IRQn 1:
void NMI_Handler(void)
{
/* USER CODE BEGIN NonMaskableInt_IRQn 0 */
/* USER CODE END NonMaskableInt_IRQn 0 */
HAL_RCC_NMI_IRQHandler();
/* USER CODE BEGIN NonMaskableInt_IRQn 1 */
while (1)
{
}
/* USER CODE END NonMaskableInt_IRQn 1 */
}
Good luck!
Regards
/Peter
2022-02-01 01:50 AM
thanks @Peter BENSCH ! you saved the day! many thanks again🙏 🙏 🙏