Skip to main content
Associate III
November 17, 2024
Solved

Question about SAR ADC in STM32H753

  • November 17, 2024
  • 6 replies
  • 1233 views

Questions:

1. Does STM32H753 have three independent 16-bit SAR ADC modules?

    Any other STM32 parts also have 16-bit SAR ADC modules?

2. Can a selected channel in each 16-bit SAR ADC module (Totally 3 selected channel in the 3 modules) be sampled simultaneously under the same clock rate?

3. How are the Direct /Fast /Slow channels in SAR ADC defined?

4. Which STM32H753 is used in NUCLEO board? (VI, ZI, AI......)

Thanks,

Rong

 

This topic has been closed for replies.
Best answer by AScha.3

1. look in ds. + yes, see cpu selection tool.

2. yes

3. see in ds . The analog mux makes some channels a little bit faster - or slower.

4. just check from the boards avail.

6 replies

AScha.3
AScha.3Best answer
Super User
November 17, 2024

1. look in ds. + yes, see cpu selection tool.

2. yes

3. see in ds . The analog mux makes some channels a little bit faster - or slower.

4. just check from the boards avail.

If you feel a post has answered your question, please click on " Best Answer ".
Associate III
November 17, 2024

1. look in ds. + see cpu selection tool.

Below shows  having 3 of16-bit ADCs - Are they independent?

Below shows STM32H753ZI has 2 direct channels, 9 fast channels, 17 slow channels.

                                              Are they independent? Or only  2 direct channels independent?

RongShengWang_0-1731878041001.png

Thanks

Rong

 

AScha.3
Super User
November 18, 2024

>Below shows  having 3 of16-bit ADCs - Are they independent?

yes.

> Are they independent? Or only  2 direct channels independent?

yes, independent .

 

see AN5354 :

AScha3_0-1731911953589.png

You should read yourself, see rm :

AScha3_1-1731912272489.png

So 1+2 can work in dual mode...but also separate.

If you feel a post has answered your question, please click on " Best Answer ".