cancel
Showing results for 
Search instead for 
Did you mean: 

STM32_Programmer_CLI fails to flash

JBill.10
Associate III

Using the STM32 CLI on Windows:

STM32_Programmer_CLI.exe c port=swd reset=HWrst -e all -d my_filename.hex -v -s -g

 

This just prints:

JBill10_0-1731965731898.png

 

If I remove the -d option, it performs the erase, so I know it can talk to the chip.  I have tried the verbosity options, they do not print any additional output.

All features work fine on Linux, using the same hardware.  It looks like a bug with the Windows build of the CLI.

 

 

1 REPLY 1
JBill.10
Associate III

This bug is present in 2.16.0 as well.

I also tried 2.15.0, which doesn't even print the banner, it just immediately crashes.