2024-10-29 04:55 AM
Question about the SPI communication clock
Is it possible to output the SPI clock all the time, not just when reading and writing data?
Solved! Go to Solution.
2024-10-29 05:01 AM - edited 2024-10-29 05:02 AM
No.
This is fundamental to the way SPI works - the Master only generates clocks during a transfer.
https://en.wikipedia.org/wiki/Serial_Peripheral_Interface
Why do you feel a need to do this?
2024-10-29 05:01 AM - edited 2024-10-29 05:02 AM
No.
This is fundamental to the way SPI works - the Master only generates clocks during a transfer.
https://en.wikipedia.org/wiki/Serial_Peripheral_Interface
Why do you feel a need to do this?
2024-10-29 05:43 AM
@pass3master if that's answered your question, please mark the solution:
https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
It seems you have already started a follow-on thread on this:
2024-10-29 03:55 PM
Sorry for the late reply. Your answer solved the issue so I will close it.