cancel
Showing results for 
Search instead for 
Did you mean: 

Question about SAR ADC in STM32H753

RongShengWang
Associate III

Questions:

1. Does STM32H753 have three independent 16-bit SAR ADC modules?

    Any other STM32 parts also have 16-bit SAR ADC modules?

2. Can a selected channel in each 16-bit SAR ADC module (Totally 3 selected channel in the 3 modules) be sampled simultaneously under the same clock rate?

3. How are the Direct /Fast /Slow channels in SAR ADC defined?

4. Which STM32H753 is used in NUCLEO board? (VI, ZI, AI......)

Thanks,

Rong

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

1. look in ds. + yes, see cpu selection tool.

2. yes

3. see in ds . The analog mux makes some channels a little bit faster - or slower.

4. just check from the boards avail.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

6 REPLIES 6
AScha.3
Chief III

1. look in ds. + yes, see cpu selection tool.

2. yes

3. see in ds . The analog mux makes some channels a little bit faster - or slower.

4. just check from the boards avail.

If you feel a post has answered your question, please click "Accept as Solution".

1. look in ds. + see cpu selection tool.

Below shows  having 3 of16-bit ADCs - Are they independent?

Below shows STM32H753ZI has 2 direct channels, 9 fast channels, 17 slow channels.

                                              Are they independent? Or only  2 direct channels independent?

RongShengWang_0-1731878041001.png

Thanks

Rong

 

>Below shows  having 3 of16-bit ADCs - Are they independent?

yes.

> Are they independent? Or only  2 direct channels independent?

yes, independent .

 

see AN5354 :

AScha3_0-1731911953589.png

You should read yourself, see rm :

AScha3_1-1731912272489.png

So 1+2 can work in dual mode...but also separate.

If you feel a post has answered your question, please click "Accept as Solution".

Hello @RongShengWang 

This thread is related to a previous thread: https://community.st.com/t5/stm32-mcus-boards-and-hardware/which-mcu-in-stm32-family-is-the-best-selection-for-using-sar-16/td-p/740651

Please accept as solution the comment that answered your question in that thread.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

.1. What means "ADC1 and ADC "tightly coupled"? Can they be coupled and also decoupled?

 2. All ADCs have 2 Direct channels. What does "direct" mean?

3. Can all ADC sampling be simultaneously under the same clock?

Thanks, 

Minor corrections to the previous question submission:

1. What means "ADC1 and ADC2 "tightly coupled"?

2. Can they be coupled and also decoupled?

3. All ADCs have 2 Direct channels. What does "direct" mean?

4. Can all ADC's channels sampling be simultaneously (one channel in each SAR ADC at a time) under the same clock rate?

Thanks, 

Peter