2024-07-04 10:31 PM
Hello.
I am testing QSPI indirect mode using STM32G474 and STM32H753.
However, I found a weird operation of QUADSPI_BK1_IO3 pin.
Other pins are OK, but QUADSPI_BK1_IO3 is high states as in the redboxes.
It should be low states (0).
I have tested in STM32G474 and STM32H753.
Both are the same.
Plz let me know how to solve this issue.
JG
2024-07-08 01:49 AM
Hello @junggun and welcome to the Community
Which pin are you using for the QUADSPI_BK1_IO3?
Which device is connected to the Quadspi interface?
Could you please check the QSPI Configuration may these examples can help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-11 11:27 AM - edited 2024-09-11 11:32 AM
Hey, we suffer from the same issue in our design. We are using pin PD13 as IO3 in QUADSPI interface and observing a high level state after the first transaction (while it should be low). The slave device is XA7A100T FPGA (no internal or external pull up). Can you please advice us what can we do to solve it?
Note that we use STM32H743VIH6 in the design
Thanks
2024-09-17 03:52 AM
Hello @Adielfr ,
Could you please check the GPIO configuration, for that I recommend you to take a look at AN4760 section GPIOs configuration.
Please refer "Recommended PCB routing guidelines for STM32H74xI/G and STM32H75xI/G devices" for QUADSPI Interface signal layout guidelines to check your PCB.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.