2020-05-24 9:47 PM
Hi,Master:
Platform: STM32F301K8U
CPU clock frequency:72M
As shown in the figure, the original analog video signal (PA7 pin) is compared with DAC1_CH1 through a comparator, and a pulse sequence with a slightly changed duty cycle and period is output. ).
my question:
How to control PA8 (or PA9 / PA10) to output a pulse sequence that is inverse to this pulse sequence, but the phase shift should not exceed 0.25us? I now capture the input of PA3 and control the PWM output of PA8 in its interrupt, resulting in the output waveform always being slower than PA2 (much greater than 0.25us).
Thank you very much.
Solved! Go to Solution.
2020-05-24 11:30 PM
> I now capture the input of PA3
Is it externally connected to PA2? Fine, then you can use timer 2 input capture 3 and 4 DMA requests to control any GPIO pin you like, provided the necessary resources, TIM2 channels 3 and 4 and DMA1 channels 1 and 7 are free.
volatile uint32_t pa8_low = (1 << 24);
volatile uint32_t pa8_high = (1 << 8);
DMA1_Channel1->CMAR = (uint32_t)&pa8_low;
DMA1_Channel1->CPAR = (uint32_t)&GPIOA->BSRR;
DMA1_Channel1->CNDTR = 1;
DMA1_Channel1->CCR =
DMA_CCR_MSIZE_1 | // memory size 32 bits
DMA_CCR_PSIZE_1 | // peripheral size 32 bits
DMA_CCR_CIRC | // circular mode
DMA_CCR_DIR | // memory to peripheral
DMA_CCR_EN; // enable channel
TIM2->CCMR2 =
TIM_CCMR2_CC3S_1 | // 10: CC3 channel is configured as input, IC3 is mapped on TI4
TIM_CCMR2_CC4S_0; // 01: CC4 channel is configured as input, IC4 is mapped on TI4
TIM2->CCER =
TIM_CCER_CC3E | // enable capture on channel 3
TIM_CCER_CC4E | // enable capture on channel 4
TIM_CCER_CC4P; // invert capture edge on channel 4
TIM2->DIER = TIM_DIER_CC3DE|TIM_DIER_CC4DE;
TIM2->CR1 = TIM_CR1_CEN;
2020-05-24 11:30 PM
> I now capture the input of PA3
Is it externally connected to PA2? Fine, then you can use timer 2 input capture 3 and 4 DMA requests to control any GPIO pin you like, provided the necessary resources, TIM2 channels 3 and 4 and DMA1 channels 1 and 7 are free.
volatile uint32_t pa8_low = (1 << 24);
volatile uint32_t pa8_high = (1 << 8);
DMA1_Channel1->CMAR = (uint32_t)&pa8_low;
DMA1_Channel1->CPAR = (uint32_t)&GPIOA->BSRR;
DMA1_Channel1->CNDTR = 1;
DMA1_Channel1->CCR =
DMA_CCR_MSIZE_1 | // memory size 32 bits
DMA_CCR_PSIZE_1 | // peripheral size 32 bits
DMA_CCR_CIRC | // circular mode
DMA_CCR_DIR | // memory to peripheral
DMA_CCR_EN; // enable channel
TIM2->CCMR2 =
TIM_CCMR2_CC3S_1 | // 10: CC3 channel is configured as input, IC3 is mapped on TI4
TIM_CCMR2_CC4S_0; // 01: CC4 channel is configured as input, IC4 is mapped on TI4
TIM2->CCER =
TIM_CCER_CC3E | // enable capture on channel 3
TIM_CCER_CC4E | // enable capture on channel 4
TIM_CCER_CC4P; // invert capture edge on channel 4
TIM2->DIER = TIM_DIER_CC3DE|TIM_DIER_CC4DE;
TIM2->CR1 = TIM_CR1_CEN;
2020-05-24 11:45 PM
Can't you simply use an invertor as an external chip?
Otherwise, you'd need to us COMP->TIM1_IC1, set TIM1 to slave Reset mode using TI1FP1 as TRGI and then generate any required sequence on TIM1_CH2 which is PA9 .
Of course that would reset the output generation upon any input edge, no sophisticated discrimination is possible at that stage. There would be some delay involved, too, probably 2-3 TIM1 input clock cycles.
JW
2020-05-26 5:06 AM
This method looks very good, thank you for your idea, I will try.
2020-05-26 5:09 AM
This method should also look great. I need to get familiar with the slave mode control of the timer. Berendi also provides a good idea. I will try your ideas. Thank you for your help. Thank you for your efforts!
2020-05-30 8:51 PM
Hi, berendi
Now I still have problems:
Since PA2 did a comparison output and could not be mapped to time2 ch3, then now only the red line can be captured for DMA control PA8 output. But TI4FP3 and TI4FP4 are all homologous, and there is no way to do a rising edge capture and a falling edge capture.
Thank you very much.
2020-05-30 8:52 PM
2020-05-30 10:27 PM
Hi,waclawek
The slave mode reset can only trigger the counter reset. Now let the PA9 output follow PA2 / PA3 (duty cycle and period are slightly changed dynamically), how to define the TIM1_CH2 output comparison value?
Thank you very much.
2020-05-30 11:03 PM
Yes there is. That's why TIM_CCER_CC4P is set, to invert the capture edge, i.e. capture on falling edge on CH4 only.
2020-05-31 3:31 AM
As I've said, there' s no sophisticated control possible.
JW