2019-11-24 12:57 AM
What is wrong with my code? The code never hits the turn on led part when I press the B1-USER1 button. From the board manual there is a LED on PD13 and the user push button on PA0.
#include "stm32f4xx.h"
GPIO_InitTypeDef GPIO_InitDef;
int main(void)
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
GPIO_InitDef.GPIO_Pin = GPIO_Pin_13;
GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitDef.GPIO_OType = GPIO_OType_PP;
GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOD, &GPIO_InitDef);
GPIO_InitDef.GPIO_Pin = GPIO_Pin_0;
GPIO_InitDef.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitDef.GPIO_OType = GPIO_OType_PP;
GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOA, &GPIO_InitDef);
while(1) {
// If button on PA0 is pressed
if (!GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_0))
{
// Turn on LED
GPIO_SetBits(GPIOD, GPIO_Pin_13);
}
else
{
// Turn off LED
GPIO_ResetBits(GPIOD, GPIO_Pin_13);
}
}
}
Solved! Go to Solution.
2019-11-24 1:46 AM
> GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_UP;
The button switches to VDD (and to GND, as is the "usual" case).
So, you have to set pull down, not pullup.
JW
2019-11-24 1:46 AM
> GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_UP;
The button switches to VDD (and to GND, as is the "usual" case).
So, you have to set pull down, not pullup.
JW