cancel
Showing results for 
Search instead for 
Did you mean: 

Programming error - STM32F030C6T6 on custom board

XooM
Senior

 

 

1000088845.jpg

 

14 REPLIES 14

I am using STM32F030C6T6.
I have a working circuit board.
I am trying to connect to it to put a new program in it.
The code was protected, I tried to remove the protection.
Now when I try to program, I get different warnings.
I don't know exactly what information you want from me.

>>I don't know exactly what information you want from me.

To present the context better, just throwing error screens in a post is not adequate.

Just pressing buttons isn't going to solve hardware issues.

So perhaps a schematic, how things are wired up, how things are powered.. What equipment you have, and experience using it.

You have NRST and BOOT0 wired? Behaviour changes with BOOT0=HIGH rather than running your code.

This is a authentic ST-LINK, or boot-leg one ?

The board's working properly?

>>I get different errors every time I try. Can you help with remote desktop?

Not paid enough to get that involved, plus this does suggest a hardware issue

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@XooM wrote:


I don't know exactly what information you want from me.


So, again, look at the Posting Tips - they tell you the information to provide:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@XooM wrote:

I have a working circuit board.


So what board is it - an ST board? a 3rd-party product? a custom design?

If it's not an ST board, show the schematic.

 

What are you using to do the programming - a genuine ST-Link? a clone ST-Link? other?

How are you connecting it the target - proper connectors? a lash-up of loose wires ... ??

 

Maybe also provide some good, clear photographs of your setup.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I am using original St-LINK/V2.

SWDIO
SWCLK
GND
VDD
NRST
Connected..

This is not an ST card.. It is a card using STM32F030C6T6..
The card was programmed by someone else.
I wanted to change the program in STM32 and program it myself.
And I started getting these errors.
I have programmed other stm32 cards before.

Select connection mode "Under reset". Make sure that NRST pin of the STM32 is connected to the ST-LINK.