cancel
Showing results for 
Search instead for 
Did you mean: 

Program update

GauravK
Senior

Hi,

1. is there any tool (GUI) to update program using executable?

2. How to have different modes of programming? (UART/ USB/ sd card)

3. Bootloader mentions: USB OTG FS (PA11/12) in Device mode (DFU: device firmware upgrade). Can external HS phy in FS as a device be used to update program?

 

16 REPLIES 16
mƎALLEm
ST Employee

Hello,


1. is there any tool (GUI) to update program using executable?


Using STM32CubeProgrammer tool

SofLit_0-1718375908892.png

 


2. How to have different modes of programming? (UART/ USB/ sd card)


Read AN2606 STM32 microcontroller system memory boot mode / Read the table " configuration in system memory boot mode" that corresponds to your device. It describes the different resources and which interface is used for bootloader for that device. SD card is not a part of the ST bootloader you need to develop it yourself.


3. Bootloader mentions: USB OTG FS (PA11/12) in Device mode (DFU: device firmware upgrade). Can external HS phy in FS as a device be used to update program?


Same answer as 2.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
GauravK
Senior

Hi, reading on program update is ongoing.

I tried using STM32CubeProgrammer and was able to program using ST-Link. 

but I tried USB FS device with DFU, and STM32CubeProgrammer was able to detect USB and when connect is pressed...the bottom bar keeps on searching and never finishes...this is with STM32F469 discovery kit.

I tried loading "DFU_standalone" also but could see same.

Please any suggestions?

What about boot pin? How you did manage it? & Reset?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
GauravK
Senior

on kit I see boot 0 and boot 1 are to GND through resistors, I was not able to change those.

Also I tried pressing RESET button, nothing happened

I didn't go for having USB FS connected and re-plugging ST-Link cable, since I read board should be powered before connecting USB.

Reading is on-going, if any suggestions from experts, can speed-up our understanding

The features and functions of the ROM will be limited. It's aimed at production programing or debricking in the field. 

For a better, more tailored, user experience you code your own loader with the rich features you want. One that implements DFU, or MSC for a drag-n-drop update, does serial XMODEM from a terminal app, or checks an SD Card for an update image.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
GauravK
Senior

I changed Boot0 to 3.3V and was able to do "Start Program" from CubeProgrammer, USB was detected and download looked complete. But it didn't boot to flash.

So changed again boot0 to GND, but don't see the program updated...

Is anything missed?

I used .elf files, 2 numbers, both having different LEDs to be toggled


So changed again boot0 to GND, but don't see the program updated...


Did you reset the MCU after changing boot0 to GND?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
GauravK
Senior

yes reset press tried, also USB cable re-insertion tried.

 

GauravK
Senior

CubeProg logs for USB DFU, verify program is failing

  18:47:37 : UR connection mode is defined with the HWrst reset mode
  18:47:37 : USB speed   : Full Speed (12MBit/s)
  18:47:37 : Manuf. ID   : STMicroelectronics
  18:47:37 : Product ID  : STM32  BOOTLOADER
  18:47:37 : SN          : 2057355C5231
  18:47:37 : DFU protocol: 1.1
  18:47:37 : Board       : --
  18:47:37 : Device ID   : 0x0434
  18:47:37 : UPLOADING OPTION BYTES DATA ...
  18:47:37 :   Bank          : 0x00
  18:47:37 :   Address       : 0x1fffc000
  18:47:37 :   Size          : 16 Bytes
  18:47:37 :   Bank          : 0x01
  18:47:37 :   Address       : 0x1ffec008
  18:47:37 :   Size          : 4 Bytes
  18:47:37 : UPLOADING ...
  18:47:37 :   Size          : 1024 Bytes
  18:47:37 :   Address       : 0x8000000
  18:47:37 : Read progress:
  18:47:37 : Data read successfully
  18:47:37 : Time elapsed during the read operation is: 00:00:00.003
  18:47:58 : Memory Programming ...
  18:47:58 : Opening and parsing file: usb_fs_update_test_01 - led1.elf
  18:47:58 :   File          : usb_fs_update_test_01 - led1.elf
  18:47:58 :   Size          : 27.00 KB 
  18:47:58 :   Address       : 0x08000000 
  18:47:58 : Erasing memory corresponding to segment 0:
  18:47:58 : Erasing internal memory sectors [0 1]
  18:47:58 : sector 0000 does not exist
  18:47:58 : sector 0001 does not exist
  18:47:58 : Download in Progress:
  18:47:58 : File download complete
  18:47:58 : Time elapsed during download operation: 00:00:00.240
  18:47:58 : Verifying ...
  18:47:58 : Read progress:
  18:47:58 : Error: Data mismatch found at address  0x08000DD0 (byte = 0x00 instead of 0x40)
  18:47:58 : Error: Download verification failed
  18:48:13 : Disconnected from device.

 whereas from ST Link its ok

  18:45:48 : UR connection mode is defined with the HWrst reset mode
  18:45:49 : ST-LINK SN  : 066CFF575285514867153350
  18:45:49 : ST-LINK FW  : V2J44M29
  18:45:49 : Board       : 32F469IDISCOVERY
  18:45:49 : Voltage     : 3.25V
  18:45:49 : SWD freq    : 4000 KHz
  18:45:49 : Connect mode: Normal
  18:45:49 : Reset mode  : Software reset
  18:45:49 : Device ID   : 0x434
  18:45:49 : Revision ID : Rev A
  18:45:49 : Debug in Low Power mode is not supported for this device.
  18:45:49 : UPLOADING OPTION BYTES DATA ...
  18:45:49 :   Bank          : 0x00
  18:45:49 :   Address       : 0x40023c14
  18:45:49 :   Size          : 8 Bytes
  18:45:49 : UPLOADING ...
  18:45:49 :   Size          : 1024 Bytes
  18:45:49 :   Address       : 0x8000000
  18:45:49 : Read progress:
  18:45:49 : Data read successfully
  18:45:49 : Time elapsed during the read operation is: 00:00:00.007
  18:45:51 : Memory Programming ...
  18:45:51 : Opening and parsing file: usb_fs_update_test_01 - led3.elf
  18:45:51 :   File          : usb_fs_update_test_01 - led3.elf
  18:45:51 :   Size          : 27.00 KB 
  18:45:51 :   Address       : 0x08000000 
  18:45:51 : Erasing memory corresponding to segment 0:
  18:45:51 : Erasing internal memory sectors [0 1]
  18:45:51 : Download in Progress:
  18:45:52 : File download complete
  18:45:52 : Time elapsed during download operation: 00:00:00.902
  18:45:52 : Verifying ...
  18:45:52 : Read progress:
  18:45:52 : Download verified successfully 
  18:46:09 : Disconnected from device.