cancel
Showing results for 
Search instead for 
Did you mean: 

stm32U545RE_Q RTC wake up from standby mode

dlagyals
Associate II

I am using an stm32U545RE_Q and want to put my device into standby mode and then periodically wake it up (every 10s). but it doesn't work

 

Am I missing something or how am I supposed to continue from here?

스크린샷 2025-03-24 144302.png스크린샷 2025-03-24 144307.png

 

/* USER CODE BEGIN Header */

/**

******************************************************************************

* @file : main.c

* @brief : Main program body

******************************************************************************

* @attention

*

* Copyright (c) 2025 STMicroelectronics.

* All rights reserved.

*

* This software is licensed under terms that can be found in the LICENSE file

* in the root directory of this software component.

* If no LICENSE file comes with this software, it is provided AS-IS.

*

******************************************************************************

*/

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"

#include "icache.h"

#include "memorymap.h"

#include "rtc.h"

#include "usart.h"

#include "gpio.h"

 

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#include <string.h>

#include <stdio.h>

/* USER CODE END Includes */

 

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

 

/* USER CODE END PTD */

 

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

 

/* USER CODE END PD */

 

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

 

/* USER CODE END PM */

 

/* Private variables ---------------------------------------------------------*/

 

/* USER CODE BEGIN PV */

 

/* USER CODE END PV */

 

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void SystemPower_Config(void);

/* USER CODE BEGIN PFP */

 

/* USER CODE END PFP */

 

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

 

/* USER CODE END 0 */

 

/**

* @brief The application entry point.

* @retval int

*/

int main(void)

{

 

/* USER CODE BEGIN 1 */

 

/* USER CODE END 1 */

 

/* MCU Configuration--------------------------------------------------------*/

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* USER CODE BEGIN Init */

__HAL_RCC_PWR_CLK_ENABLE();

HAL_PWR_EnableBkUpAccess();

__HAL_RCC_RTC_ENABLE();

__HAL_RCC_RTC_CONFIG(RCC_RTCCLKSOURCE_LSE);

/* USER CODE END Init */

 

/* Configure the System Power */

SystemPower_Config();

 

/* Configure the system clock */

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

 

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_USART1_UART_Init();

MX_RTC_Init();

MX_ICACHE_Init();

/* USER CODE BEGIN 2 */

uint8_t buffer[256];

uint8_t count=0;

if(__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) !=RESET)

{

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF);

 

char *str ="Wake up form the STANDBY MODE\r\n\n";

HAL_UART_Transmit(&huart1, (uint8_t*)str, strlen(str), 10);

 

for(int i=0; i<20; i++)

{

HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);

HAL_Delay(200);

}

 

//HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN2);

 

HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

}

__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc,RTC_FLAG_WUTF);

 

char *str ="Enter the STANDBY MODE\r\n\n";

HAL_UART_Transmit(&huart1, (uint8_t*)str, strlen(str), 10);

 

for(int i=0; i<5; i++)

{

HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);

HAL_Delay(1000);

}

 

//HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_HIGH_1);

/*if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 10000, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0) != HAL_OK)

{

Error_Handler();

}*/

 

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{sprintf((char *)buffer, "Loop! %d\r\n", ++count);

HAL_UART_Transmit(&huart1, buffer, strlen((char *)buffer), 100);

HAL_Delay(1000);

if (count==5)

{ char *str2 ="STANDBY MODE is ON\r\n\n";

HAL_UART_Transmit(&huart1, (uint8_t*)str2, strlen(str2), 10);

HAL_SuspendTick();

HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0x2805, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);

__HAL_RCC_PWR_CLK_ENABLE ();

HAL_PWR_EnterSTANDBYMode();

}

 

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

}

/* USER CODE END 3 */

}

 

/**

* @brief System Clock Configuration

* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE4) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_MSI;

RCC_OscInitStruct.LSIState = RCC_LSI_ON;

RCC_OscInitStruct.MSIState = RCC_MSI_ON;

RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;

RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;

RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV1;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2

|RCC_CLOCKTYPE_PCLK3;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

Error_Handler();

}

}

 

/**

* @brief Power Configuration

* @retval None

*/

static void SystemPower_Config(void)

{

 

/*

* Switch to SMPS regulator instead of LDO

*/

if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)

{

Error_Handler();

}

/* PWR_S3WU_IRQn interrupt configuration */

HAL_NVIC_SetPriority(PWR_S3WU_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(PWR_S3WU_IRQn);

/* USER CODE BEGIN PWR */

/* USER CODE END PWR */

}

 

/* USER CODE BEGIN 4 */

void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc) {

HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);

__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(hrtc, RTC_FLAG_WUTF);

}

 

/* USER CODE END 4 */

 

/**

* @brief This function is executed in case of error occurrence.

* @retval None

*/

void Error_Handler(void)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

__disable_irq();

while (1)

{

HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);

}

/* USER CODE END Error_Handler_Debug */

}

 

#ifdef USE_FULL_ASSERT

/**

* @brief Reports the name of the source file and the source line number

* where the assert_param error has occurred.

* @param file: pointer to the source file name

* @param line: assert_param error line source number

* @retval None

*/

void assert_failed(uint8_t *file, uint32_t line)

{

/* USER CODE BEGIN 6 */

/* User can add his own implementation to report the file name and line number,

ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

 

 

 

----> This is my code

1 REPLY 1
KDJEM.1
ST Employee

Hello @dlagyals;

 

Please use </> button to share your code. See this post.

For the RTC issue, First of all I recommend you to look at this FAQ and check how to calculate WakeUpCounter. 

KDJEM1_0-1742812279520.png

 

Second, I advise you to get inspired from an available example to check your code like as RTC_LowPower_STANDBY_WUT.
This example describes how to periodically enter and wake up from STANDBY mode thanks to the RTC Wake-Up Timer (WUT).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.