cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with data reception via USART2 on STM32F429ZI microcontroller

Emanuele78
Associate III

I tried to follow exactly what was indicated in the following tutorial https://www.youtube.com/embed/JWOV4j5fCS4?cc_load_policy=1&autoplay=1&list=PL8n_tqwYdzVAd_OxaKnfxBrvcGwR8kSJo, but despite the serial port being connected, I am not receiving the data on the console that I send through the micro.

What could be the cause? In the attached screenshots, you can find the settings and the code from main.c.

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @Emanuele78 ,

This is because on NUCLEO-F429ZI USART2 is not connected to VCP (Virtual Comport).

SofLit_0-1731405492268.png

You need to use USART3 then.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello @Emanuele78 ,

This is because on NUCLEO-F429ZI USART2 is not connected to VCP (Virtual Comport).

SofLit_0-1731405492268.png

You need to use USART3 then.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.