cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with USART on Nucleo-F401RE

david027
Associate II

Hi, I am pretty new to STM32 MCUs and I am having trouble with USART communication. I would like to send a message from Nucleo-F401RE to raspberry pi 3b+, and then to display that message in terminal on raspberry. I have tried to use USART2 for this but it didn't work, then i read that USART2 is used when i connect Nucleo to the laptop so i changed the code to use USART1 and it still doesn't work.

I have tested the USART2 with the advanced serial monitor on the laptop and it works properly.

Bellow are the functions in main.c and uart.c that i am currently using

This is the function uart.c, for some reason i couldn't post it as the attachment:

#include "moduli/uart.h" #include "stm32f401xe.h" #define BUFFER_SIZE 64 static uint8_t ring_buffer[BUFFER_SIZE]; static uint8_t rb_write; static uint8_t rb_read; void uart1_init() { /* * PA9 --> USART1 TX (AF7) * PA10 --> USART1 RX (AF7) */ RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; RCC->APB2ENR |= RCC_APB2ENR_USART1EN; // Init GPIO GPIOA->MODER &= ~(0b11 << (9 * 2) | 0b11 << (10 * 2)); GPIOA->MODER |= (0b10 << (9 * 2) | 0b10 << (10 * 2)); GPIOA->AFR[1] &= ~(0xF << ((9 - ‌‌ * 4) | 0xF << ((10 - ‌‌ * 4)); GPIOA->AFR[1] |= (7 << ((9 - ‌‌ * 4) | 7 << ((10 - ‌‌ * 4)); // Init USART1 USART1->CR1 &= ~(1 << 15); // OVER8 = 0 (16 samples) USART1->CR1 &= ~(1 << 12); // 8 data bits USART1->CR1 &= ~(1 << 10); // no parity USART1->CR1 |= (1 << 5); // RXNE interrupt enable USART1->CR1 |= (1 << 3); // TE USART1->CR1 |= (1 << 2); // RE // Baudrate: 9600 @ 42 MHz USART1->BRR = (273 << 4) | 7; USART1->CR1 |= (1 << 13); // USART enable NVIC->ISER[1] |= (1 << (37 - 32)); // USART1 IRQ } void uart1_send_data(unsigned char data) { while (!(USART1->SR & (1 << 6))); // TXE USART1->DR = data; } void uart1_send_data_array(unsigned char *data, unsigned int size) { for (int i = 0; i < size; i++) { uart1_send_data(*data++); } } void uart1_echo() { if (rb_read == rb_write) return; while (ring_buffer[rb_read] != '\0') { uart1_send_data(ring_buffer[rb_read]); rb_read = (rb_read + 1) % BUFFER_SIZE; } } void USART1_IRQHandler(void) { if ((USART1->SR & (1 << 5)) != 0) { // RXNE ring_buffer[rb_write] = USART1->DR; rb_write = (rb_write + 1) % BUFFER_SIZE; ring_buffer[rb_write] = '\0'; } }
View more

 

Can somebody help me with this?

Thanks in advance.

 

Code formatting applied - please see How to insert source code for future reference.

0 REPLIES 0