cancel
Showing results for 
Search instead for 
Did you mean: 

PC13 GPIO Usage recommendation on STM32G491MCT

Mahalakshmisudhakar
Associate II

Hi @Peter BENSCH 

I am using the controller STM32G491MCT controller for my development project.I am running out of GPIO pins.I am planning to use PC13 to drive the level translator SN74LV4T125 for sending serial clock and data signals from my master device to the slave module. It is given in the datasheet that there is some limitations in the PC13,PC14 & PC15 pins which cannot be used for driving high speed signals.

Could you please confirm that can I use the PC13 for driving level translator?

Anticipating the earliest response!

Thanks in advance

5 REPLIES 5
Danish1
Lead III

For anyone to be able to answer that question correctly, we would need to know how you intend to use the pin PC13, and possibly the timing requirements for the "serial clock and data signals".

Will PC13 only drive the /OE pin on the level-translator? If so, would it be a problem if it were slow, perhaps taking a microsecond for the change to happen?

Or do you intend for PC13 to carry serial clock and/or data? (In which case there is a recommendation not to exceed 2 MHz; how does that compare to your intended bit-rate).


@Mahalakshmisudhakar wrote:

It is given in the datasheet that there is some limitations in the PC13,PC14 & PC15 pins which cannot be used for driving high speed signals


It gives you a lot more detail than that:

AndrewNeil_0-1739350772893.png

which is, surely, enough to answer the question?

 


@Mahalakshmisudhakar wrote:

Could you please confirm that can I use the PC13 for driving level translator?


Ask yourself:

  • Does this unnamed  "level translator" require more than 3mA drive current ?
  • Does its load capacitance exceed 20pF ?
  • Does your signal exceed 2MHz ?

that should answer your question.

 

BTW: Note that the datasheet is incorrect in saying, "the switch only sinks (sic) a limited amount of current" - they mean sources.

See: https://community.st.com/t5/stm32-mcus-products/stm32f030-pc13-14-15-current-sink-limits/m-p/721081/highlight/true#M261048

@STTwo-32 - another datasheet needing correction.


@Andrew Neil wrote:


It gives you a lot more detail than that:


Here:

AndrewNeil_1-1739351686815.png

https://www.st.com/resource/en/datasheet/stm32g491mc.pdf#page=62

Billy OWEN
ST Employee

Hi @Mahalakshmisudhakar 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

@Billy OWEN - I hope the Online Support Team will feed back here as this is quite a common question and, as noted, the datasheets can be confusing on this issue.